Site Search | Product Search | IA Global Search |
... ZW-5000@: 0645817 to ZW-7000@: 0825817 to * Serial number format @@@@@@@ (1)(2)(3)(4)(5)(6)(7) Digit Meaning Displayed characters Sequential number from 0001 0001 to 9999 (5) Month of manufa...
https://www.omron-ap.co.th/data_pdf/mnu/z362-e1-09_zw-_000.pdf
...is based on the object dictionary of the CAN application protocol. All objects are assigned a 4-digit hex index and comprise the following areas. Index Area Description 0000 hex to 0FFF hex D...
https://www.omron-ap.co.th/data_pdf/mnu/z363-e1-07_zw-_000.pdf
...adding 1 to the result. 00000001 (= 1) Invert all bits 11111110 Plus 1 11111111 (=-1) The first digit is used to judge whether the number is positive or negative. • When 0: Positive number (o...
...adding 1 to the result. 00000001 (= 1) Invert all bits 11111110 Plus 1 11111111 (=-1) The first digit is used to judge whether the number is positive or negative. • When 0: Positive number (o...
....2 < Screw: M5 or M6 > [ Unit : mm ] F3SG-4RA-25-01TS Series Dimension A C+23 Dimension C 4-digit...
https://www.omron-ap.co.th/data_pdf/mnu/z380-e1-04_f3sg-4ra____-25-01ts.pdf
...ll be set if processing ended in an error. • These bits are reserved. The diagnostic results (4-digit hexadecimal) are attached. --1 word If communications diagnostics are disabled, 0000 hex ...
https://www.omron-ap.co.th/data_pdf/mnu/z389-e1-12_v780-hmd68-etn-__-s.pdf
... 46.35 31.4 38 150 max. 150 max. 56.5 56.5 73 2-M4 10 P 3.95 50
https://www.omron-ap.co.th/data_pdf/mnu/z391-e1-03_f3sg-4ar____-25-02ts.pdf
...ron Microscan’s serial configuration commands begin with a single “K” character followed by a 3-digit numeric character, comma-separated command fields, and an initializing command, as follow...
https://www.omron-ap.co.th/data_pdf/mnu/z392-e1-08_v430-f.pdf
...er events by the system in advance according to the type of event. Controller event codes are 8-digit hexadecimal values. NX-series Communication Control Unit Built-in Function User's Manual ...
https://www.omron-ap.co.th/data_pdf/mnu/z396-e1-03_nx-csg.pdf
...and Data Password ARRAY [] OF BYTE 4 bytes Specifies the access password to set in the Tag in 8-digit hexadecimal (32 bits) (00000000 hex). Locking: The access password to set in the RF Tag t...
https://www.omron-ap.co.th/data_pdf/mnu/z402-e1-10_v780-hmd68-e__-__.pdf
...0 max. 46.7 32 38 250 max. 10 P 250 max. a. di 5.7 3 6. 5.7 34.4 2-M5 or M6
https://www.omron-ap.co.th/data_pdf/mnu/z405-e1-08_f3sg-sr_pg.pdf
...es number (numInfo ber of images) that were needed to get a Good Read result. The output is a 3 digit number. ABCDE,F010 3 Code Position Coordinates I/O - Output Object Outputs the coordinate...
https://www.omron-ap.co.th/data_pdf/mnu/z407-e1-06_v3_0-f_v4_0-f.pdf
...adding 1 to the result. 00000001 (= 1) Invert all bits 11111110 Plus 1 11111111 (=-1) The first digit is used to judge whether the number is positive or negative. • When 0: Positive number (o...
https://www.omron-ap.co.th/data_pdf/mnu/z408-e1-10_fhv7h.pdf
... ETC and TIME must be set to DISP. ↓ ▼ or ▲ Key YEAR Press the SET/REC/STOP key, then, the last digit number at the lower 2010 row starts blinking. ↓ SET/REC/STOP Key YEAR The value increases...
https://www.omron-ap.co.th/data_pdf/mnu/z410-e1-04_zn-ctx21_kmx21.pdf
... ・ Settings of Control Word C1 (C1: 5010) Word Setting (Data format) Communications port No. (1-digit hex) Serial port No. (1-digit hex) C1 Unit address of communications partner (2...
https://www.omron-ap.co.th/data_pdf/mnu/z414-e1-01_v320-f_v420-f_v430-f.pdf
...memory Successful USB error Copy error Inspection error Mode error After "E-" is displayed, a 4-digit code is shown in the order of upper two digits → lower two digits (repeated). Chapter 10 ...
https://www.omron-ap.co.th/data_pdf/mnu/z415-e1-10_mx-z2000h-v1.pdf
...g Mark string “MX-Z2000” on the upper level of the work, and the Year/Month/Day, as well as a 4-digit counter on the lower level of the work. Create the string “MX-Z2000” block and the Year/M...
https://www.omron-ap.co.th/data_pdf/mnu/z416-e1-10_mx-z2000h-v1.pdf
... in the command. Word D9000 D9001 D9002 Setting (Data format) Number of bytes of send data (4-digit hex) 1st and 2nd bytes of send data (4-digit hex) 3rd and 4th bytes of send data...
https://www.omron-ap.co.th/data_pdf/mnu/z431-e1-01_v330-f_v430-f.pdf
...ersal Product Code) is a fixed length, numeric, continuous symbology. UPC can have two- or five-digit supplemental bar code data following the normal code. The UPC Version A (UPC, A) symbol i...
https://www.omron-ap.co.th/data_pdf/mnu/z432-e-06 (84-9000400-02-e)_v3_0-f_v4_0-f.pdf
...se will be displayed. * As shown in the example figure on the right, by typing [1] as the first digit of the “Assembly Number”, all the possible Assembly Numbers beginning with that ...
https://www.omron-ap.co.th/data_pdf/mnu/z441-e-01_f430-f.pdf