| Site Search | Product Search | IA Global Search |
...-contrast monochrome EL dis- play for the NT631-ST211@-EV2, an STN color LCD display with back- light for the NT631C-ST141@-EV2, and a TFT color LCD high-definition display for NT631C-ST153@-...
https://www.fa.omron.com.cn/data_pdf/mnu/v063-e1-05_nt631_631c_setup.pdf
...1-2 Section Functions of the NT21, NT31/NT31C and NT631/NT631C 18 Touch switches can be made to light or flash in accordance with the status of a host bit in the same way as lamps. The follow...
https://www.fa.omron.com.cn/data_pdf/mnu/v069-e1-03_nt21_nt31_nt631.pdf
... Disturbance from noise or irregularity in hardware are possible causes. If alarm flag does not light after removing CPU error Unlit Unlit --- --- --- --- Error detected in the watchdog timer...
https://www.fa.omron.com.cn/data_pdf/mnu/w124-05_c200h-ts001_002_101_102.pdf
... Lit when other PC Link Units are operating properly. Not lit when an error has occurred. ERROR Light when a unit number is set incorrectly; flashes when an error has occurred on the links be...
https://www.fa.omron.com.cn/data_pdf/mnu/w135-03_c200h-lk401_c500-lk009-v1.pdf
.... . . . . . . . . . . . 80 5-1 Error Indications When an error occurs, the ERROR indicator will light and the error flag will turn ON. Error information is then output to IR word n+5 when REA...
https://www.fa.omron.com.cn/data_pdf/mnu/w141-04_c200h-ct001-v1_ct002.pdf
...vices, like the Photoelectric Switch and Proximity Switch shown below, use other means, such as light or inductance, in order to get information about the equipment being monitored. Photoelec...
https://www.fa.omron.com.cn/data_pdf/mnu/w302-e1-15_c200hx_hg_he_setup.pdf
... input IN2 Lit when external control input IN2 is ON. 01234567 External output These indicators light when the corresponding external output (0 through 7) is ON. Indicators Rotary switches Ex...
https://www.fa.omron.com.cn/data_pdf/mnu/w311-02_c200h-ct021.pdf
...ernet Unit. The node number must still be set from 01 to 7E, however, or the ERC indicator will light. Note Turn OFF the power supply before setting the node number. Setting the Local IP Addr...
https://www.fa.omron.com.cn/data_pdf/mnu/w343-e1-07_cs1w_cj1w-etn.pdf
...ore color Dot marking Dot color Pin No. Core color Dot marking Dot color 1Light brown ■Black 21 Light brown ■■■Black 2Red22Red 3 Yellow Black 23 Yellow Black 4Red24Red 5Light green Black...
https://www.fa.omron.com.cn/data_pdf/mnu/w347-e1-06_c200hw_cqm1-drt_drt1.pdf
...ergency stop to the input common and turn it ON. If it is not connected, the ERC indicator will light. Operation will be normal, how- ever, for all axes that are used. Unit Number Setting Swi...
https://www.fa.omron.com.cn/data_pdf/mnu/w376-e1-08_cs1w_nc.pdf
...nd mount the Board correctly. The SYSMAC LINK Support Board is faulty. If the indicators do not light when the Board is mounted in another computer, replace the SYSMAC LINK Support Board. Lit...
https://www.fa.omron.com.cn/data_pdf/mnu/w390-01_3g8f7-slk11-e_21-e.pdf
... OPEN button PB1 0.00 STOP button PB2 0.01 CLOSE button PB3 0.02 Car detection sensor SEN1 0.03 Light detection sensor SEN2 0.04 Upper limit LS LS1 0.05 Lower limit LS LS2 0.06 Device Contact...
https://www.fa.omron.com.cn/data_pdf/mnu/w461-e1-06_cp1l_cp1e.pdf
...1E/CP2E CPU Units are backed up in the built-in EEPROM or Flash Memory. The BKUP indicator will light on the front of the CPU Unit when the backup operation is in progress. Do not turn OFF th...
https://www.fa.omron.com.cn/data_pdf/mnu/w483-e1-08_cp1e_cp2e.pdf
...log Output or Analog I/O Units, the ERC or ERH indi- cators on the front panel of the Unit will light. 7-2-1 Indicators and Error Flowchart Indicators LED Meaning Indicator Operating status R...
https://www.fa.omron.com.cn/data_pdf/mnu/w490-e1-03_cj1w-ad0__-___da0_mad42.pdf
...tus of the Temperature Control Unit, as explained in the following table. The Output Indicators light to indicate when the corresponding Temperature Control Unit output is ON. 2-3-1 Part Name...
https://www.fa.omron.com.cn/data_pdf/mnu/w491-e1-03_cj1w-tc003_004_103_104.pdf
...mmunication error occurs at a Slave Unit, the NS indicator on the front of the Master Unit will light and the seven-segment display will show d9. At the same time, the representative communic...
https://www.fa.omron.com.cn/data_pdf/mnu/w493-e1-03_cj1w-crm21.pdf
...d its service life and this flag changes to TRUE. At the same time, the ERC indicator will also light. Although this has no effect on communications and other functions, replace the Unit prom...
https://www.fa.omron.com.cn/data_pdf/mnu/w494-e1-04_cj1w-scu_2.pdf
... NX-PG0122, NX-PG0232-5, NX-PG0242-5, NX-PG0332-5, NX-PG0342-5 Change Details The shape of the light emitting part of each indicator has been changed from a square to a penta- gon. Below is ...
https://www.fa.omron.com.cn/data_pdf/mnu/w524-e1-11_nx-ec0_ecs_pg.pdf
...on •Locations outdoors subject to direct wind and rain •Locations subject to strong ultraviolet light •Always install the product with sufficient surrounding space to allow for adequate heat ...
https://www.fa.omron.com.cn/data_pdf/mnu/w557-e2-10_ny532.pdf
... ON the following power supplies. •Slave unit power supply (The PWR indicator on the slave will light when the power supply turns ON.) •Slave I/O power supply •Controller power supply Compare...
https://www.fa.omron.com.cn/data_pdf/mnu/w562-e1-06_ny532_ny512.pdf