| Site Search | Product Search | IA Global Search |
... to this output. Input 1 Input 1 and Input 2 are bi-directional and isolated. Each input can be wired as sinking (NPN) or sourcing (PNP). Wire these according to the output device connected t...
...Internal Circuit Details Input 1 and Input 2 are bi-directional and isolated. Each input can be wired as sinking (NPN) or sourcing (PNP). Wire these according to the output device connected t...
...ls The Power ON Input and the UPS Mode Input are bi-directional and isolated. Each input can be wired as sinking (NPN) or sourcing (PNP). Wire these according to the output device connected t...
https://www.omron-ap.co.in/data_pdf/mnu/w556-e2-08_ny512-1_00.pdf
...ls The Power ON Input and the UPS Mode Input are bi-directional and isolated. Each input can be wired as sinking (NPN) or sourcing (PNP). Wire these according to the output device connected t...
https://www.omron-ap.co.in/data_pdf/mnu/w557-e2-10_ny532.pdf
... bandwidth for part of the communications path may be exceeded, depending on how the network is wired. This may prevent the tag data links from operating correctly. If this occurs, either cal...
https://www.omron-ap.co.in/data_pdf/mnu/w563-e1-08_ny532_ny512.pdf
...Load Cell Input Unit connections, the compatibility is confirmed in the following conditions. • Wired with a 6-wire connection • 6-core shielded cables are used. • One end of the shield wire ...
https://www.omron-ap.co.in/data_pdf/mnu/w565-e1-06_nx-rs.pdf
...e wires is to insert the ferrules into the terminal holes. Wiring Terminals The terminals to be wired are as follows. • I/O power supply terminals • I/O terminals Applicable Wires You can con...
https://www.omron-ap.co.in/data_pdf/mnu/w566-e1-07_nx-ts_hb.pdf
...ture prevents troubles caused by a terminal block that is attached to a wrong place after it is wired. When you remove the terminal blocks from the CPU Unit for wiring, be careful not to swap...
https://www.omron-ap.co.in/data_pdf/mnu/w578-e1-15_nx1p2.pdf
...d the COM terminals on the lower terminal block are internally connected, but they must also be wired externally. 07 + 8-point Output Units (Terminal Block is not removable) Input Wiring Diag...
...t to right and top to bottom. The flow is different from that for circuits that consist of hard-wired control relays. For example, when the diagram in figure A is executed by the CPU Unit, po...
...ot apply stress to the cable after you have connected the wires. The Power and I/O connector is wired. NY-series NYE Industrial Panel PC Hardware User's Manual (W634) 5-29 5 Installation 5-3-...
...n-collector outputs should not be short-circuited. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing in the same duct may cause ...
https://www.omron-ap.co.in/data_pdf/mnu/z197-e1-04_zx-l-n.pdf
...ted. • Use the power supply within the rated load. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
...ted. • Use the power supply within the rated load. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
https://www.omron-ap.co.in/data_pdf/mnu/z209-e1-03_zs-mdc.pdf
...ted. • Use the power supply within the rated load. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
https://www.omron-ap.co.in/data_pdf/mnu/z210-e1-04_zs-dsu.pdf
...ted. • Use the power supply within the rated load. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
https://www.omron-ap.co.in/data_pdf/mnu/z236-e1-08_zs-hl.pdf
...n-collector outputs should not be short-circuited. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
https://www.omron-ap.co.in/data_pdf/mnu/z237-e1-03_zj-sd.pdf
...r when using the S8M. Minor fire may possibly occur. Ensure that input and output terminals are wired correctly. Increases in the temperature of internal parts resulting from heating of wirin...
...ted. • Use the power supply within the rated load. • High-voltage lines and power lines must be wired separately from this product. Wiring them together or placing them in the same duct may c...
https://www.omron-ap.co.in/data_pdf/mnu/z263-e1-05_zx-gt.pdf
...must be checked by OMRON. • This error will occur if the power supply and load circuits are not wired correctly. See 3-3-1 Wiring the Power Supply and Load Circuits on page 24 and 3-3-5 Wirin...