| Site Search | Product Search | IA Global Search |
...share a ground line with other devices, or connect it to a structural beam of a building. Doing so will have the opposite effect, and may adversely affect the Sensor. S3D2 Resistance: 50 Ω Ca...
https://www.fa.omron.co.jp/data_pdf/cat/s3d2_ds_e_7_2_csm511.pdf
... normally cleared when the power supply is turned ON, the setting of a parameter can be changed so that errors are not cleared. (This is not possible for the S8AS2-@@-@SN.) Refer to the S8AS2...
https://www.fa.omron.co.jp/data_pdf/cat/s8as2_t243-e1_2_1_csm1132735.pdf
...is function is provided to disable cutoff operations for 40 ms after the branch outputs turn ON so that cutoff operations will not occur for large inrush currents. Safety Circuits 60 Temperat...
https://www.fa.omron.co.jp/data_pdf/cat/s8as_t228-e1_9_6_csm1381.pdf
...Flexibility/Select the Optimum Output Capacity DC-DC UPS AC-AC UPS • This type of UPS is large, so it must be installed outside the control panel or it requires excessive space inside the con...
https://www.fa.omron.co.jp/data_pdf/cat/s8ba_u700-e1_2_6_csm1042404.pdf
...due to malfunction of the UPS or another external factor affecting the UPS operation. Not doing so may result in serious accidents. Carry the unit considering its weight and balance, and plac...
https://www.fa.omron.co.jp/data_pdf/cat/s8ba_u701-e1_4_9_csm1042516.pdf
...cteristics of fuses and the operating characteristics of breakers and select fuses and breakers so that external fuses will not burn out or breakers will not operate due to inrush current. Ri...
https://www.fa.omron.co.jp/data_pdf/cat/s8fs-g_t207-e1_6_1_csm1056419.pdf
...nd 7-8 are shorted. Removal of the connector may deteriorate the output stability and accuracy, so be sure to perform the connection of +S and -S terminals. Never connect a load to the output...
https://www.fa.omron.co.jp/data_pdf/cat/s8jx_t041-e1_20_5_csm2005.pdf
...re proper heat dissipation to increase the long-term reliability of the S8M. 3. Install the S8M so that the air flow circulates around it, because the S8M is designed to radiate heat by means...
https://www.fa.omron.co.jp/data_pdf/cat/s8m_t232-e1_3_4_csm2006.pdf
...02 Power Supply To Be Connected The power consumption of the S8T-DCBU-02 is approximately 10 W, so make sure that the output capacity of the connected Power Supply is sufficient. If the S8T-D...
https://www.fa.omron.co.jp/data_pdf/cat/s8t-dcbu-02_t234-e1_10_3_csm138.pdf
...mA max. Note: 1. Alarm signal output is not equipped with an internal current limiting circuit, so be sure that the current flowing to the alarm signal output terminals does not exceed 50 mA....
https://www.fa.omron.co.jp/data_pdf/cat/s8v-cp_t226-e1_5_1_csm1074611.pdf
...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...
https://www.fa.omron.co.jp/data_pdf/cat/s8v-cp_t227-e1_2_1_csm1074606.pdf
...rotection (B) Face-up mounting Consider the possibility of an overvoltage and design the system so that the load will not be subjected to an excessive voltage even if the feedback circuit in ...
https://www.fa.omron.co.jp/data_pdf/cat/s8vk-g_t056-e1_7_1_csm1012199.pdf
...d by installing it properly and sufficiently considering heat dissipation. • Install the S8VK-R so that the air flow circulates around it, because the S8VK-R is designed to radiate heat by me...
https://www.fa.omron.co.jp/data_pdf/cat/s8vk-r_t059-e1_4_8_csm1013796.pdf
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.fa.omron.co.jp/data_pdf/cat/s8vk-s_t205-e1_2_1_csm1050136.pdf
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.fa.omron.co.jp/data_pdf/cat/s8vk-t_t061-e1_11_1_csm1021435.pdf
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.fa.omron.co.jp/data_pdf/cat/s8vk-x_t210-e1_2_2_csm1060688.pdf
... Protection Output voltage (V) Consider the possibility of an overvoltage and design the system so that the load will not be subjected to an excessive voltage even if the feedback circuit in ...
https://www.fa.omron.co.jp/data_pdf/cat/s8vs_t026-e1_8_1_csm2022.pdf
...ay occur. Motor M Note: To prevent the buzzer sounding when power is turned ON, install a timer so that the buzzer sounds only when the timer’s contacts are closed. 5 SAO Operation Settings ...
https://www.fa.omron.co.jp/data_pdf/cat/sao_ds_e_5_4_csm390.pdf
...ed. The calculation method is as follows: The PICK UP index scale value is between 1.0 and 3.0, so calculate the voltage multiplying factor for both 1.0 and 3.0. 15 V (Operating value)/1 (PIC...
https://www.fa.omron.co.jp/data_pdf/cat/sdv_ds_e_6_6_csm392.pdf
...M_SensingBand_CN_E_1_2 !WARNING Do not touch the terminals while power is being supplied. Doing so may possibly result in electric shock. Do not attempt to disassemble, repair, or modify the ...
https://www.fa.omron.co.jp/data_pdf/cat/sensingband_cn_e_1_2_csm524.pdf