| Site Search | Product Search | IA Global Search |
...ser ter- minal, an executing program, or a pendant. Once this request has been made, the button light blinks, and the operator must press the button for high power to be applied. The default ...
https://www.omron.com.tw/data_pdf/mnu/i602-e-03_smartcontroller_ex.pdf
........................................................................... 15 Reference Guide for Light Source Setup ...............................................................................
https://www.omron.com.tw/data_pdf/mnu/i853-e-03_tm_conveyor_tracking.pdf
...canner A control device for controlling the angle of rotation of the mirror that reflects laser light for scanning the position where the laser light is irradiated. It utilizes the h...
https://www.omron.com.tw/data_pdf/mnu/o052-e1-02_ck_m_ck3w.pdf
...ayed in the Value Column. 17 Check that Operation mode switch on Photoelectric Sensor is set to Light ON (factory setting). Make sure that there is no sensing object in front of Photoelectric...
... 3 2 1 0 Control Output1 0:OFF 1:ON Control Output2 0:OFF 1:ON Reserved 0 Instability Alarm(Non-Light Receiving) 0:Stable 1:Unstable Instability Alarm(Light Receiving) 0:Stable 1:Uns...
https://www.omron.com.tw/data_pdf/mnu/p665-e1-01_e3z_gx-ilm.pdf
... 3 2 1 0 Control Output1 0:OFF 1:ON Control Output2 0:OFF 1:ON Reserved 0 Instability Alarm(Non-Light Receiving) 0:Stable 1:Unstable Instability Alarm(Light Receiving) 0:Stable 1:Uns...
...on •Outdoor locations directly subject to wind or rain •Locations subject to strong ultraviolet light •Take appropriate and sufficient countermeasures when installing systems in the following...
https://www.omron.com.tw/data_pdf/mnu/v082-e1-10_ns_ext_operation_manu.pdf
...e port number. 2 Port Reset Setting Restarts the selected port. 3 Exit Display The display will light in green when the selected port has been restarted normally. Remarks * When using this Sm...
https://www.omron.com.tw/data_pdf/mnu/v087-e1-01_ns5_ns8_ns10_ns12-v1_refer.pdf
... Click Create two labels as shown on the right by referring to“9. Displaying a Text”. [Label] Æ“Light Alarm Display” [Tile Background] ÆUncheck the box. [Label] Æ“High Alarm Display” [Til B k...
https://www.omron.com.tw/data_pdf/mnu/v089-e1-02a_ns-cxdc1-v1.pdf
...tion Locations outdoors subject to direct wind and rain Locations subject to strong ultraviolet light Locations subject to dust Locations subject to direct sunlight Locations subject to splas...
https://www.omron.com.tw/data_pdf/mnu/v108-e1-22_nb3q_nb5q_nb7w_nb10w.pdf
...s that are outdoors and subject to direct wind and rain Locations subject to strong ultraviolet light Locations subject to dust Locations subject to direct sunlight Locations subject to splas...
https://www.omron.com.tw/data_pdf/mnu/v126-e1-07_na-rtld.pdf
...ion. An abnormal operation may result in a serious accident. Since this product emits a visible light that may have an adverse effect on the eyes, do not stare directly into the ...
https://www.omron.com.tw/data_pdf/mnu/v__0-f__f__0-f__inst-83-9500134-01.pdf
... Disturbance from noise or irregularity in hardware are possible causes. If alarm flag does not light after removing CPU error Unlit Unlit --- --- --- --- Error detected in the watchdog timer...
https://www.omron.com.tw/data_pdf/mnu/w124-05_c200h-ts001_002_101_102.pdf
... Lit when other PC Link Units are operating properly. Not lit when an error has occurred. ERROR Light when a unit number is set incorrectly; flashes when an error has occurred on the links be...
https://www.omron.com.tw/data_pdf/mnu/w135-03_c200h-lk401_c500-lk009-v1.pdf
.... . . . . . . . . . . . 80 5-1 Error Indications When an error occurs, the ERROR indicator will light and the error flag will turn ON. Error information is then output to IR word n+5 when REA...
https://www.omron.com.tw/data_pdf/mnu/w141-04_c200h-ct001-v1_ct002.pdf
... n + 1 begins operation. Dur- ing operation, the RUN indicator on the Data Setting Console will light and camoutputswill turnONandOFF according to the data that is set. When this flag turns O...
https://www.omron.com.tw/data_pdf/mnu/w224-02_c200h-cp114.pdf
... input IN2 Lit when external control input IN2 is ON. 01234567 External output These indicators light when the corresponding external output (0 through 7) is ON. Indicators Rotary switches Ex...
https://www.omron.com.tw/data_pdf/mnu/w311-02_c200h-ct021.pdf
...d A424, bit 09 will turn ON. For the Serial Communications Unit, the RDY or ERC indicators will light. C200HX/HG/HE: Set to 1 (ON) when an error is detected in the Pro- tocol data checksum. A...
https://www.omron.com.tw/data_pdf/mnu/w344-e1-18_cx-protocol.pdf
...ore color Dot marking Dot color Pin No. Core color Dot marking Dot color 1Light brown ■Black 21 Light brown ■■■Black 2Red22Red 3 Yellow Black 23 Yellow Black 4Red24Red 5Light green Black...
https://www.omron.com.tw/data_pdf/mnu/w347-e1-06_c200hw_cqm1-drt_drt1.pdf
...ounter. Note a) When interrupt inputs are used in interrupt input mode, the indica- tor may not light even when the interrupt condition is met if the in- put is not ON long enough. b) Input i...
https://www.omron.com.tw/data_pdf/mnu/w377-e1-04_cpm2c_s.pdf