| IAグローバル検索 |
...ed for a variety of purposes including dust level setting, alarm output, timed measurement, and so forth. Triggers can be input to initiate monitoring when necessary and alarms can be output ...
...t having to take a robot out of production. The onscreen display includes a virtual robot stick so users can control the robot just as they would control a physical robot. In addition to the ...
... • Do not bend a wire past its natural bending radius or pull on it with excessive force. Doing so may cause the wire disconnection. • Do not insert more than one wire into each terminal inse...
https://www.fa.omron.co.jp/data_pdf/cat/a22n_m22n_a30n_a254-e1_4_13_csm1045427.pdf
...rodes must be cleaned. !WARNING Do not touch the terminals while power is being supplied. Doing so may possibly result in electric shock. Do not attempt to disassemble, repair, or modify the ...
https://www.fa.omron.co.jp/data_pdf/cat/electrodecommodity_cn_e_3_3_csm15.pdf
...e switched. Either AC or DC load voltages can be used. Transistor output There are no contacts, so high-speed, high-frequency switching is possible. Only DC can be switched and the capacity i...
https://www.fa.omron.co.jp/data_pdf/cat/h3_h5_timer_selection_guide_l130-e1_2_1_csm1129246.pdf
...ices. Integration of the Construction Process simplifies the process of implementing automation so that users can automate their sites exactly to their needs. Together, these two “integration...
https://www.fa.omron.co.jp/data_pdf/cat/robot-integrated-controller_i856-e1_3_5_csm1104446.pdf
... not use the product outdoors or in environments exposed to direct sunlight. ・ Install the unit so that air can flow freely through its cooling vents. ・ Install the product away from high-v...
https://www.fa.omron.co.jp/data_pdf/closed/mnu/fz-m08_inst-1636843-6f.pdf
.... The C16P and C4K do not. For those models which have the switch, care must be taken to set it so that it corresponds with the direction of the I/O Connecting Cable. If the switch is set in ...
https://www.fa.omron.co.jp/data_pdf/closed/mnu/w167-e1-04a_c20p_c28p_c40p_c60p.pdf
... Precautions ! WARNING Never attempt to disassemble the PC while power is being supplied. Doing so may result in serious electrical shock or electrocution. ! WARNING Never touch any of the te...
https://www.fa.omron.co.jp/data_pdf/closed/mnu/w175-e1-04a_c20h_c28h_c40h_c60h.pdf
... this program is controlled. It also explains how to convert ladder diagrams into mnemonic code so that the programs can be entered using a Programming Console. Section 5 Instruction Set desc...
https://www.fa.omron.co.jp/data_pdf/closed/mnu/w176-e1-04a_c20h_c28h_c40h_c60h.pdf
...eing supplied. In addition, do not turn on electricity in the state that founded a cover. Doing so may result in electric shock. Provide safety measures in external slave units, including the...
https://www.fa.omron.co.jp/data_pdf/mnu/crt1series(safetyprecautions)_inst-2826512-8a.pdf
...nnector before connecting it. Do not force the connector if it cannot be inserted easily. Doing so may result in damage. 2) Do not place heavy objects on top of the USB-Serial Conversion Cabl...
https://www.fa.omron.co.jp/data_pdf/mnu/e58-cifq2_inst-g.pdf
...(connecting portion) of this product directly or allow it to come in contact with metals. Doing so may cause internal data to be erased or destroyed by static electricity. · Do not allow the ...
https://www.fa.omron.co.jp/data_pdf/mnu/fz-mem2g_inst-1897588-7d.pdf
... it well to ensure that you are using the K3HB correctly. • Keep this manual in a safe location so that it is available for reference when required. Visual Aids The following headings appear ...
...G Do not touch any of the terminals or terminal blocks while the power is being supplied. Doing so may result in electric shock. Do not attempt to take any Unit apart while the power is being...
https://www.fa.omron.co.jp/data_pdf/mnu/nj-cpuseries(safetyprecautions)_inst-3105385-9b.pdf
...way to the Unit on the far right side of the Controller. A step in a procedure 1 Join the Units so that the connectors fit exactly. Hook Indicates a procedure. Hook holes Connector 4-3 Mo u n...
https://www.fa.omron.co.jp/data_pdf/mnu/o037-e1-08_nj501-r__0.pdf
...way to the Unit on the far right side of the Controller. A step in a procedure 1 Join the Units so that the connectors fit exactly. Hook Indicates a procedure. Hook holes Connector 4-3 Mo u n...
https://www.fa.omron.co.jp/data_pdf/mnu/o049-e1-05_nj501_ac1_rl4_rx4.pdf
...意味は、以下のとおりです。 設定値 00Hex 01Hex 意味 • IO-Link モード時有効:IO-Link デバイスに出力無効通知を行います。 • SO モード時有効:出力値をクリア(OFF)します。 • IO-Link モード時無効:...
https://www.fa.omron.co.jp/data_pdf/mnu/sbcd-350n_gx_xwt-id_od.pdf
...attempt to take any Unit apart or touch any internal parts while power is being supplied. Doing so may result in electric shock. !WARNING Do not touch any of the terminals or terminal blocks ...
https://www.fa.omron.co.jp/data_pdf/mnu/w345-e1-12_cj1w-ad_da_mad.pdf
...etwork. !WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing so may result in electric shock. xxvi 3 Safety Precautions !WARNING Do not touch any of the ter...
https://www.fa.omron.co.jp/data_pdf/mnu/w394-e1-16_cs_cj_nsj.pdf