Primary Contents

IAグローバル検索結果

国/地域選択

IAグローバル検索
結果 4941 - 496025803
3Z4S-LE VS-TEV Series Ultra-high-resolution Telece...

...d iris adjustment may become loose or come off due to shock or vibration during transportation, so please be caution when unpacking. last update: March 10, 2025...

https://www.omron-ap.com/products/family/3692/lineup.html

E8FC IoT Flow Sensors/Features | OMRON Industrial ...

...g position Angle adjustment up to 330° After fastening to the adapter, you can adjust the angle so that the display is easy to see. 180° reverse display The display can rotate 180°. Useful fu...

https://www.omron-ap.com/products/family/3720/feature.html

E8PC IoT Pressure Sensors/Features | OMRON Industr...

...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON You can use a rise in hyd...

https://www.omron-ap.com/products/family/3721/feature.html

TM Series Collaborative Robots/Features | OMRON In...

...and acts as a beacon to help the robot navigate. The robot uses a Landmark as a reference point so it can better locate objects within the workspace. During high-mix, low-volume production wi...

https://www.omron-ap.com/products/family/3739/feature.html

FHV7 Series Smart Camera/Features | OMRON Industri...

...ase of the shutter. Easy filter replacement The light cover and optical filter are replaceable, so you don't need to prepare a protection cover against dirt. Single camera for inspecting vari...

https://www.omron-ap.com/products/family/3740/feature.html

R89F-M AC Free Input Axial Fans/Features | OMRON I...

... which allows multiple input voltage ranging 100 to 240 VAC. Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...

https://www.omron-ap.com/products/family/3759/feature.html

R89F-D DC Axial Fans/Features | OMRON Industrial A...

...te: May 6, 2021 For less design effort DC Axial Fans R89F-DS Not affected by changes in voltage so no need to redesign for export Also, the service life of the fans themselves increased by tw...

https://www.omron-ap.com/products/family/3760/feature.html

R88M-1A[] / R88D-1SAN[]-ECT AC Servo System 1S-ser...

...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION • You can pickup the product safely with Safely-Limited Spe...

https://www.omron-ap.com/products/family/3776/feature.html

E3AS-HL / F / L Series Distance-settable Photoelec...

...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...

https://www.omron-ap.com/products/family/3779/feature.html

S8V-CP DC Electronic Circuit Protector (24 VDC 4 O...

...oducts with safety outputs of which voltage, current, and power are limited to a certain level, so that not to cause an electric shock or fire,” and is evaluated by UL1310. For the UL Class 2...

https://www.omron-ap.com/products/family/3780/feature.html

E2E NEXT Proximity Sensor/Features | OMRON Industr...

...cements in as little as 10 seconds*1 using e-jig Using e-jig eliminates the need for adjustment so that anyone can install in the same position. Easily upgrade existing facilities to enable “...

https://www.omron-ap.com/products/family/3790/feature.html

K7GE-MG Insulation Resistance Monitoring Device/Fe...

...ts frequency of automatic measurement allows for understanding the degradation trend, which was so far difficult. K7GE proposes a new way of monitoring insulation. Highly reproducible measure...

https://www.omron-ap.com/products/family/3811/feature.html

FH-SMD 3D Robot Vision System/Features | OMRON Ind...

...etect parts inside the bin. To detect these parts, an operator must reposition items in the bin so that the parts are within the field of view. Cameras installed at the robot arms can reduce ...

https://www.omron-ap.com/products/family/3827/feature.html

E3X-ZV / MZV Smart Fiber Amplifier Units/Features ...

...arts feeders, roll presses for secondary batteries, assembly machines for digital products, and so on to detect the presence or absence of workpieces. However, many customers are using fiber ...

https://www.omron-ap.com/products/family/3831/feature.html

K7TM Heater Condition Monitoring Device/Features |...

...ate of change of the heater resistance value and monitor the state and tendency of each heater, so it is possible to determine when replacement is necessary, so it is unplanned while...

https://www.omron-ap.com/products/family/3855/feature.html

FS Series (GigE Vision CMOS Line Sensor Camera) Gi...

...ifications.       Incorrect wiring can lead to failure. *2. Do not connect the shell, for doing so can cause failure or malfunction. *3. When wiring a camera, be sure to refer to its specific...

https://www.omron-ap.com/products/family/3873/lineup.html

STC Series (USB3.0 Series) USB3.0 Series/Lineup | ...

...      documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: October 1, 2024...

https://www.omron-ap.com/products/family/3874/lineup.html

STC Series (USB3.0 Remote Head Camera) USB3.0 Remo...

...      documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. Model Applicable Model General Specifications S-Mount (M12...

https://www.omron-ap.com/products/family/3876/lineup.html

STC Series (CoaXPress) CoaXPress/Lineup | OMRON In...

...ation documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. Note. STC-M[]S502CXP121/-S[]S510CXP62/-M[]S510CXP121/-M[]S...

https://www.omron-ap.com/products/family/3877/lineup.html

STC Series (Opt-C:Link) Opt-C:Link/Lineup | OMRON ...

...      documents, for faulty wiring can cause failure. Note. Do not connect the shell, for doing so can cause failure or malfunction. last update: January 5, 2023...

https://www.omron-ap.com/products/family/3878/lineup.html

結果 4941 - 496025803

国/地域選択

Related Contents