| IAグローバル検索 |
...換 - ● セーフティデータロギング - ● オンライン機能確認 - ● 使用可能なセーフティI/Oユニット/ターミナル NX-SI ● ● NX-SO ● ● GI-SMD/SID - ● 接続可能なCPUユニット NX502 CPUユニット ● ● NX102 ...
https://www.fa.omron.co.jp/product/selection/32/func_spec.html
...ライトカーテン F3SG-SRシリーズ NXシリーズ 通信コントロールユニット/セーフティコントロールユニット NX-CSG / SL5 / SI / SO 非常停止用押ボタンスイッチ(φ22/φ25) A22NE-PD / A22NE-P / A22E セーフ...
...ライトカーテン F3SG-SRシリーズ NXシリーズ 通信コントロールユニット/セーフティコントロールユニット NX-CSG / SL5 / SI / SO 非常停止用押ボタンスイッチ(φ22/φ25) A22NE-PD / A22NE-P / A22E セーフ...
...with the spot beam type sensor "E3AS-HF" Can stably detect only workpieces when it is installed so that the optical axis passes through the gap between the roller conveyors. 搬送 稼働率向上 D...
...ired for connection to a variety of devices. Reduced Wiring Signal line wiring has been reduced so that the Terminal can be mounted closer to sensors and other devices. Relay Box not Required...
https://www.fa.omron.com.cn/data_pdf/closed/cat/compobus_s_q103-e1-07.pdf
... the heat sinks of the G32X-A or the G3PX. 3. Insert the Cartridge into the opening of the G3PX so that the letters on the Cartridge and those on the G3PX are in the same direction and sides ...
https://www.fa.omron.com.cn/data_pdf/closed/cat/g3px-eh(n)_ds_csm187.pdf
...Cautions WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing so may result in electric shock. WARNING Do not touch any of the terminals, terminal blocks or,...
...he controller or turn the power OFF while writing or reading data to or from the product. Doing so may result in the internal data being destroyed or erased. ·Be sure to never disassemble or ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/fz-mem2g_inst-1897588-7d.pdf
...angerous parts under the cover. Do not attempt to open the cover under any circumstances. Doing so may result in injury or death and may damage the product. Never attempt to repair or disasse...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/i539-e1-03_3g3mv-pdrt2_3g3rv-pdrt2.pdf
...he ground terminal of the Power Supply Unit (CPM2C-PA201) to a ground or 100Ωor less. Not doing so may result in electric shock. !WARNING Do not attempt to take any Unit apart while the power...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w356-e1-08_cpm2c.pdf
...etwork. !WARNING Do not attempt to take any Unit apart while the power is being supplied. Doing so may result in electric shock. xxvii Safety Precautions 3 !WARNING Do not touch any of the te...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w394-e1-16_cs_cj_nsj.pdf
... high-frequency switching. Unlimited number of switching operations. Consist of semiconductors, so there is no contact erosion caused by switching. Zero cross function. No operation noise. Et...
https://www.ia.omron.com/data_pdf/guide/18/ssr_tg_e_9_12.pdf
...f the time. (2) Terminal Arrangement •Models with a signal start require three external inputs, so they have many terminals. •Models with a power supply start (H3CR-A8) are the H3CR Timers mo...
https://www.ia.omron.com/data_pdf/guide/19/timer_timeswitch_tg_e_7_5.pdf
...tput Capacity Output capacity (W) = Output voltage (V)×Load current (I) Select the Power Supply so that the maximum load capacity will be lower than the rated output capacity. Note: The outpu...
https://www.ia.omron.com/data_pdf/guide/22/powersupply_tg_e_8_4.pdf
...cation range from standard to high-capacity loads. The fixed rivet contact is usually processed so that it has a groove to eliminate compounds that may be generated as a result of switching. ...
https://www.ia.omron.com/data_pdf/guide/29/microswitch_tg_e_3_4.pdf
...-ring or a rubber diaphragm is used for sealing. The rubber seal is not externally exposed, and so resistance is provided against cutting debris from machine tools, but sand and fine shavings...
https://www.ia.omron.com/data_pdf/guide/30/limitswitch_apparatus_tg_e_3_2.pdf
...ater; however, at water treatment plants it may refer to water at a stage before it is purified so it has a broader meaning than purified water. Sewage (Sewer) Better described as a wastewate...
https://www.ia.omron.com/data_pdf/guide/33/levelapparatus_tg_e_8_2.pdf
...will weaken. The power of the release spring will become stronger than the magnetic attraction, so the armature will release and the relay will be in the relaxed state. When the armature has ...
https://www.ia.omron.com/data_pdf/guide/36/generalrelay_tg_e_10_6.pdf
...e vibration test method (JIS C0040/IEC68-2-6) and the shock test method (JIS C0041/IEC68-2-27), so that vibrations and shocks in the general specifications will not cause malfunctions. Howeve...
https://www.ia.omron.com/support/guide/26/further_information.html
...Do not operate motors that exceed the allowable capacity with G3Js connected in parallel. Doing so may result in malfunctions. Tightening Screws Be sure to tighten the screws to the specified...
https://www.omron.com.tw/data_pdf/closed/cat/g3j-t-c_g3j-t_g3j-s_g3j_cn_e_3_3_csm159.pdf