| IAグローバル検索 |
...olarity when wiring. •The rated voltage is shown on the plate on the back of the lighting unit, so be sure to use within the voltage shown. •An LED current-limiting resistor is built in,...
https://www.fa.omron.com.cn/data_pdf/cat/a3p_ds_e_9_3_csm615.pdf
...Do not wire the Switch or touch any terminal of the Switch while power is being supplied. Doing so may result in electric shock. Always use the Switch in a system that is operated directly by...
https://www.fa.omron.com.cn/data_pdf/cat/a4e_ds_e_3_4_csm1267.pdf
...L, INT, BCD, or STRING. Data configuration files required for the host computer can be created, so necessary data can be retrieved even if the SPU is mounted in a device after the PLC is alre...
https://www.fa.omron.com.cn/data_pdf/cat/cs1w-spu_cj1w-spu_v301-e1_3_1_csm1015430.pdf
...t subject the plunger to a force exceeding that shown in the corresponding diagram below. Doing so may damage the product. D5SN-S Sensors D5SN-M Sensors •If the actuator is pushed in too far,...
https://www.fa.omron.com.cn/data_pdf/cat/d5sn_d5m_d5v_x071-01.pdf
...er from entering the tubes after the Sensor is removed from its packaging. (5) Attach the tubes so that fluid flows only in the direction des- ignated by the arrows on the Sensor. Correct mea...
https://www.fa.omron.com.cn/data_pdf/cat/d6f-p_a183-e1-05.pdf
...dow. Power ON Conditions Sensing is enabled within 200 ms for the E2K-C20M@@. Design the system so that the power for the Sensor is turned ON before the power for the load. z Miscellaneous Or...
https://www.fa.omron.com.cn/data_pdf/cat/e2k-c_ds_e_6_5_csm457.pdf
...sult. The following precautions must be observed to ensure safe operation of the product. Doing so may cause damage or fire. •Do not install the product in the following locations. (1) Locati...
https://www.fa.omron.com.cn/data_pdf/cat/e2nc_e473-e1_7_1_csm1061200.pdf
...e Slit to the upper indented mounting portion of the Sensor and adjust the position of the Slit so that the Slit will be in parallel to the lens side of the Sensor. 2. Press the lower protrud...
https://www.fa.omron.com.cn/data_pdf/cat/e3c_photoelectric_operation_tg_e_7_3_csm442.pdf
...es may become immersed in oil or other liquids or where liquids may penetrate the Sensor. Doing so may result in damage from burning and fire, particularly if the liquid is flammable. 3. When...
https://www.fa.omron.com.cn/data_pdf/cat/e3s-a_ds_e_13_1_csm1296.pdf
...sity of the light received by the sensor from highly-reflective glossy packaging is too strong, so there is not enough difference in incident levels to perform color mark detection (i.e. satu...
https://www.fa.omron.com.cn/data_pdf/cat/e3s-dc_e3nx-ca_y216-e1_1_9_csm1052116.pdf
...or such purposes. The following precautions must be observed to ensure safe operation. 1. Doing so may cause damage or fire. Do not install the product in the following locations. •Locations ...
https://www.fa.omron.com.cn/data_pdf/cat/e3s-r_ds_e_10_5_csm428.pdf
...for such purposes. The following precautions must be observed to ensure safe operation. 1.Doing so may cause damage or fire. Do not install the product in the following locations. •Locations ...
https://www.fa.omron.com.cn/data_pdf/cat/e3s_ds_e_13_2_csm1308.pdf
... E3X-SD The Standard for Fiber Amplifiers with Simple Operation and High Performance ■Operation so simple that essentially anyone can use the amplifier right way. ■Immediately determine opera...
https://www.fa.omron.com.cn/data_pdf/cat/e3x-sd_e388-e1_2_1_csm2114.pdf
...cate the minimum required distance between the Sensor and the Reflector. *3. Install the Sensor so that plastic bottles are at least 500 mm from the Sensor when they pass. *4. Models with a 0...
https://www.fa.omron.com.cn/data_pdf/cat/e3z-b_ds_e_10_1_csm433.pdf
... to each other. Otherwise, mutual interference may result. •Always install the Sensor carefully so that the aperture angle range of the Sensor will not cause it to be directly exposed to inte...
https://www.fa.omron.com.cn/data_pdf/cat/e3z-ls_ds_e_9_5_csm436.pdf
..., or outdoors. Ambient Environment Do not install the product in the following locations. Doing so may result in product failure or malfunction. •Locations subject to excess dust and dirt •Lo...
https://www.fa.omron.com.cn/data_pdf/cat/e3z-lt_lr_ll_ds_e_7_5_csm2158.pdf
... flow that exceeds the rated current. If a load short circuit occurs, the output will turn OFF, so check the wiring before turning ON the power supply again. The short- circuit protection cir...
https://www.fa.omron.com.cn/data_pdf/cat/e3zm-v_e389-e1_6_3_csm2113.pdf
...nt malfunction or adverse affects on the performance or functionality of the product. Not doing so may occasionally result in faulty operation. 1. This product is specifically designed for in...
https://www.fa.omron.com.cn/data_pdf/cat/e5_n_e5_nh_e5_n-ht_cn_e_3_5_csm1373.pdf
...irection. (Maintain the specified mounting space between Controllers.) •To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. •When two or more ...
https://www.fa.omron.com.cn/data_pdf/cat/e5cn-fr_h132-e1-01.pdf
...sions E5CS 8 ■Accessories (Order Separately) Note: Do not use any other types of Sockets. Doing so will adversely affect the accuracy. Applicable Thermistors Use Element Interchangeable Therm...
https://www.fa.omron.com.cn/data_pdf/cat/e5cs_ds_e_5_3_csm211.pdf