| IAグローバル検索 |
...OMRON Corporation Industrial Automation Company No.(SO)道场-1810276 产品新闻产品停产通知发行日期 2019年3月1日电力、设备用保护装置No. 2019038C 静止型过电流继电器K2CA-R系列停产通知停产产品推...
https://www.fa.omron.com.cn/upload/alternative/201904030413426941.pdf
...OMRON Corporation Industrial Automation Company No.(SO)道场-1810276 产品新闻产品停产通知发行日期 2019年3月1日电力、设备用保护装置No. 2019038C 静止型过电流继电器K2CA-R系列停产通知停产产品推...
https://www.fa.omron.com.cn/upload/alternative/201904030416043417.pdf
...: Not compatible - : No corresponding specification * Accessories (cables and mounting brackets so on) are only for OS3101. Production is ended according to the production end of OS3101. Disc...
https://www.fa.omron.com.cn/upload/alternative/PRDN-2011195E.pdf
...In a machine operation intervention such as removing a crashed product, the machine is stopped, so there is no production. SOLUTION Yo u c a n p i c k u p t h e p r o d u c t s a f e l y w i ...
https://www.omron-ap.co.in/data_pdf/cat/1s_series_i858-e1-01.pdf
... contactor. Do not use a contactor or thermal relay which has been dropped or dismantled. Doing so may cause malfunction or a fire. Life period of contactor depends on the operating applicati...
https://www.omron-ap.co.in/data_pdf/cat/J7_j510-e2-02a+lvsg+groupcat.pdf
... c o n tr o l D i r ec t PW M CK3W-G C La s er p r ocessing En c o de r Line ar E ncoder Lase r so u r c e PWM / digital Galvo S c an n e r Galvo in te r fac e Ordering Information L as e r I...
https://www.omron-ap.co.in/data_pdf/cat/ck3w-gc_ck3w-ecs_o904-e1_1_1_csm1110780.pdf
... be replaced during power supply or operation. In addition, cable disconnections are monitored, so failures can be located easily. Remove or add units without using a programming device The d...
https://www.omron-ap.co.in/data_pdf/cat/cs1d-cpu__s_bc082s_etn21d_r103-e1_9_23_csm1004122.pdf
...cements in as little as 10 seconds*1 using e-jig Using e-jig eliminates the need for adjustment so that anyone can install in the same position. Previous models A lot of time required to adju...
https://www.omron-ap.co.in/data_pdf/cat/e2e_d121-e1_3_5_csm1067251.pdf
... detect (Fig. 1) Sensor sensor from highly-reflective glossy packaging Threshold is too strong, so there is not enough Existing challenges Incident level difference in incident levels to perf...
https://www.omron-ap.co.in/data_pdf/cat/e3s-dc_e3nx-ca_y216-e1_1_9_csm1052116.pdf
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.co.in/data_pdf/cat/e5_d-800_h226-e1_1_6_csm1057810.pdf
...ction in processing quality. • The hydraulic pressure system is divided into multiple sections, so finding degraded packing locations takes time. Solution from OMRON Temp. You can use a rise ...
https://www.omron-ap.co.in/data_pdf/cat/e8fc_e8pc_e472-e1_4_3_csm1065029.pdf
... achieved by locking and unlocking of stopper. Wiring work efficiency improvement Lock Designed so that wires are hard come out even if release levers are touched unintentionally. Work judgme...
https://www.omron-ap.co.in/data_pdf/cat/g2rv-st_g3rv-st_j265-e1_2_10_csm1121815.pdf
... prevent malfunction. Transport Do not transport the G3PE under the following conditions. Doing so may result in damage, malfunction, or deterioration of performance characteristics. • Condit...
https://www.omron-ap.co.in/data_pdf/cat/g3pe_j174-e1_2_1_csm2137.pdf
... • The transistor output of the H7CC is isolated from the internal circuitry by a photocoupler, so the transistor output can be used as both NPN and PNP output. NPN Output PNP Output Load + P...
https://www.omron-ap.co.in/data_pdf/cat/h7cc_m094-e1_2_9_csm1106903.pdf
...sier to understand, and the present value display can be switched between red, green and orange so that output status can be seen from a distance. Temperature (°C) AC power supply *2 Previous...
https://www.omron-ap.co.in/data_pdf/cat/h7cc_m095-e1_3_1_csm1106892.pdf
...open-collector output of the K7L-U/UB is isolated from the internal circuits by a photocoupler, so you can use either an NPN opencollector output or a PNP (equivalent) output. NPN Output PNP ...
https://www.omron-ap.co.in/data_pdf/cat/k7l_n211-e1_6_7_csm1050158.pdf
...erminals. • Connect a branch circuit breaker between the voltage input terminals and the wiring so that the power supply can be turned OFF immediately. • For safety, always work with the powe...
https://www.omron-ap.co.in/data_pdf/cat/km-n2_km-n3_n213-e1_3_13_csm1050147.pdf
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron-ap.co.in/data_pdf/cat/nx-tc_nx-htc_h229-e1_2_2_csm1061207.pdf
...e active CPU Unit, the standby CPU Unit takes over in an instant (using the hot standby method) so that system operation continues essentially unaffected. Other duplex variations are also pos...
https://www.omron-ap.co.in/data_pdf/cat/plc-based_process_control_p051-e1_9_17_csm2684.pdf
...ning. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.omron-ap.co.in/data_pdf/cat/s8vk-w_t219-e1_5_1_csm1066917.pdf