| IAグローバル検索 |
...K thermocouple at−200 to 1,300°C) by default. Thermocouples Resistance Thermometers E5CC/E5EC K J T R. etc. Pt JPt E5CC/E5EC Input type Sensor type Input temperature setting range in°C Input ...
https://www.omron.com.tw/data_pdf/mnu/h182-e1-01_e5cc_e5ec.pdf
...larm, HB alarm, or HS alarm turns ON. 1-1-3 Main Functions Thermocouple (temperature input): K, J, T, E, L, U, N, R, S, B, C/W, or PL II Resistance thermometer (temperature input): Pt100, JPt...
...ol method that conforms to the Modicon Company's RTU-mode Modbus Protocol (PI-MBUS-300 Revision J). Modbus is a registered trademark of Schnei- der Electric. It supports functions equivalent ...
...larm, HB alarm, or HS alarm turns ON. 1-1-3 Main Functions Thermocouple (temperature input): K, J, T, E, L, U, N, R, S, B, C/W, or PL II The sensor specifications K, J, and T can dis...
...ol method that conforms to the Modicon Company's RTU-mode Modbus Protocol (PI-MBUS-300 Revision J). Modbus is a registered trademark of Schnei- der Electric. It supports functions equivalent ...
...escription A MountingPads F Motor Cover B eAIB G Outer Arms C Cable Inlet Box H Platform D Base J Ball Joints (SpringAssembliesnot shown) E Inner Arm eAIB The power amplifiers for the Quattro...
https://www.omron.com.tw/data_pdf/mnu/i597-e-05_quattro_650h(s)_800h(s).pdf
...or scaling input B. Constant K Use steps G to I to set constant K, if required. Proceed to step J if constant K is not included in the calculation and does not, therefore, need to be set. A P...
...tor[1].AbsPhasePosOffset set value. The AMP ENAB 0 LED is turned on at that time. 2 Type the #1 j+ command from the Ter- minal. 3 Make sure that the motor is rotating. In addition, confirm th...
https://www.omron.com.tw/data_pdf/mnu/o047-e1-02_ck3w-ax.pdf
...oject file. 1 Type the #1 hmz command in the Pow- er PMAC IDE Terminal. After that, type the #1 j=10 command. 2 Confirm that the X axis is moving. Also, confirm that the value of Position #1 ...
https://www.omron.com.tw/data_pdf/mnu/o052-e1-02_ck_m_ck3w.pdf
...ing table as well as an equivalent, or the fuse that belongs to the following class: CC, CF, G, J, R or T. Item Unit Model (R88D-1SN) 55F-ECT 75F-ECT 150F-ECT Power supply capacity kVA 13.3 1...
https://www.omron.com.tw/data_pdf/mnu/r88m-1l__-1m__r88d-1sn_-ect_inst-2884903-0d_en.pdf
...(Molex製接頭) GT1-DA04MX型輸出: 0~5V、1~5V、 0~10V、-10~ +10V 輸入4點0CH 端子台型 (M3端子台) GT1-TS04T型輸入種類: R、S、K、J、T、B、 L 溫度輸入模組輸入4點 4CH (8CH) (依顯示模式而異) 0CH ...
https://www.omron.com.tw/data_pdf/mnu/sbcd-314h-tw5-01_cs1w_cj1w-drm.pdf
...d on the Memory Card. Aptvmod Attr Checklist Dir FONTS Grep Plcmon Procs Winmgr Plcmon_E Plcmon_J \ldrmt_v1 Spydidmn Procon Pbtc_4832_0101 Pbts_4832_0101 Plcd_1616_0102 \procon Plcd_1616_0202...
https://www.omron.com.tw/data_pdf/mnu/v082-e1-10_ns_ext_operation_manu.pdf
...ser account. (h) Used to delete the selected user account. (i) Used to add a new user account. (j) User account table A list of the user accounts that are currently registered is dis- played....
https://www.omron.com.tw/data_pdf/mnu/v126-e1-07_na-rtld.pdf
... Omron personnel. (i) Software program embedded by other than Omron or usage of such software. (j) Cause which could not have been foreseen with the level of science and technology at the tim...
https://www.omron.com.tw/data_pdf/mnu/v453-e1-01_nx701_nj_01_na5-_w.pdf
... four models. The C200H- TS001/002 are for use with thermocouples, and can be used with K (CA), J (IC) and L (Fe-CuNi) thermocouples. The C200H-TS101/102 are for use with platinum resistance ...
https://www.omron.com.tw/data_pdf/mnu/w124-05_c200h-ts001_002_101_102.pdf
... ParameterDislasandSettins SecU◎R34 eThissetstheintegraitime.ltisvalidonlywhenSW203-1issettoOFF(j.e.,PlD control). eThisvalueisreflectedevenwhenauto-tuning(AT)isexecuted。 SPLowerLgmit(DEspta...
https://www.omron.com.tw/data_pdf/mnu/w240-e1-01_c200h-tv.pdf
...ement on the same line, separate the state- ments with a colon (:). Example: 10 FOR L=1 TO 100: J=L*I: PRINT J: NEXT L Line No. Statement 1 Statement 2 Statement 3 Statement 4 Commen...
https://www.omron.com.tw/data_pdf/mnu/w306-03_c200h-asc11_21_31.pdf
...ation/deceleration pattern data C200HW-NC413 Sequence Data Edit Screen 1, 2, 3... 1. Click“Jump(J)”in the sequence data, positioning action, or acceleration/de- celeration data edit screen. T...
https://www.omron.com.tw/data_pdf/mnu/w324-e1-04_ws01-nctf1-e.pdf
...PMSU. Procedures for writing control temperatures and operating parameters. Temp Controller (E5_J) Protocol for controlling a E5@J Temperature Controller via the PMSU. Procedures for...
https://www.omron.com.tw/data_pdf/mnu/w344-e1-18_cx-protocol.pdf
...r Unit. •Thermocouple inputs (and measurement ranges): K (–200 to 1,300°C), K (0.0 to 500.0°C), J (-100 to 850°C), and J (0.0 to 400.0°C). •Platinum resistance thermometer inputs (an...
https://www.omron.com.tw/data_pdf/mnu/w377-e1-04_cpm2c_s.pdf