| IAグローバル検索 |
...d pull it straight. 【Note】 Do not pull out with excessive force without pressing the tab. Doing so may break the wire. Before mounting Controller side Controller side Lighting side Lighting...
https://www.omron.com.tw/data_pdf/mnu/flv-xc_ep_inst-2279564-8b.pdf
...d pull it straight. 【Note】 Do not pull out with excessive force without pressing the tab. Doing so may break the wire. Before mounting Controller side Controller side Lighting side Lighting...
https://www.omron.com.tw/data_pdf/mnu/flv-xc_s2_inst-2279615-6c.pdf
...andling ·Do not peel off or damage the waterproof sheet attached to the side of the unit. Doing so may result in dirt, dust or water droplet entering inside the device, causing a failure of t...
https://www.omron.com.tw/data_pdf/mnu/fq-cr__inst-2243166-2h.pdf
...ield of view 30 mm 115 mm Installation distance (L) (mm) Imaging range Adjust the shutter speed so that the Sensor can capture images of the measurement object at a suitable brightness. If th...
https://www.omron.com.tw/data_pdf/mnu/fq2-ch1_____-m(quickstartupguide)_inst-2269304-7a.pdf
...andling ·Do not peel off or damage the waterproof sheet attached to the side of the unit. Doing so may result in dirt, dust or water droplet entering inside the device, causing a failure of t...
https://www.omron.com.tw/data_pdf/mnu/fq2-ch1_____-m_inst-9909933-4i.pdf
...he controller or turn the power OFF while writing or reading data to or from the product. Doing so may result in the internal data being destroyed or erased. ·Be sure to never disassemble or ...
https://www.omron.com.tw/data_pdf/mnu/fz-mem16g_inst-5727687-2b.pdf
...ssibly occur due to loss of required safety functions. Wire the G9SP-series Controller properly so that the 24VDC line does NOT touch the outputs accidentally or unintentionally. Serious inju...
https://www.omron.com.tw/data_pdf/mnu/g9sp-n10s_n10d_n20s_inst-2114042-7f.pdf
...rious injury may possibly occur due to loss of required safety functions. Wire G9SX-NS□properly so that supply voltages or voltages for loads do NOT touch the safety inputs accidentally or un...
https://www.omron.com.tw/data_pdf/mnu/g9sx-nsa222-t03-__ns202-__inst-0631752-3j.pdf
... ix ■Safety Precautions CAUTION Do not touch the terminals while power is being supplied. Doing so may occasionally result in minor injury due to electric shock. Use a power supply that compl...
... Cautions WARNING Never use the product without installing protective circuit in network. Doing so may possibly cause abnormal operation, and result in serious injury, property damage, or acc...
https://www.omron.com.tw/data_pdf/mnu/h155-e1-05_devicenet_ej1.pdf
...ted to specific levels. CAUTION Do not touch the terminals while power is being supplied. Doing so may occasionally result in minor injury due to electric shock. Do not allow pieces of metal,...
https://www.omron.com.tw/data_pdf/mnu/h157-e1-08_e5cn-h_e5an-h_e5en-h.pdf
... understand this manual in order to ensure correct use. Also, store this manual in a safe place so that it can be retrieved whenever necessary. ©OMRON, 2008-2022 All rights reserved. No part ...
https://www.omron.com.tw/data_pdf/mnu/h159-e1-04_e5cn-h_e5an-h_e5en-h.pdf
... the alarm is ON and OFF when the alarm is OFF (NO: Close in Alarm). You can change the setting so that the output will be ON when the alarm is OFF and OFF when the alarm is ON (NC: Open in A...
https://www.omron.com.tw/data_pdf/mnu/h182-e1-01_e5cc_e5ec.pdf
... terminal screws to the specified torque of 0.43 to 0.58 N·m. Set the parameters of the product so that they are suitable for the system being controlled. If they are not suitable, unexpected...
... terminal screws to the specified torque of 0.43 to 0.58 N·m. Set the parameters of the product so that they are suitable for the system being controlled. If they are not suitable, unexpected...
...and other possible attacks before using this product. CAUTION Set the parameters of the product so that they are suitable for the system being controlled. If they are not suitable, unexpected...
...and other possible attacks before using this product. CAUTION Set the parameters of the product so that they are suitable for the system being controlled. If they are not suitable, unexpected...
...ange is machined into one of the pivot links. It does not rotate in relation to the pivot link, so there are no gears or belts involved. See P31 Platform on page 18. P30 Platform (P/N09730-xx...
https://www.omron.com.tw/data_pdf/mnu/i597-e-05_quattro_650h(s)_800h(s).pdf
...e 21 22 SmartController EX User's Guide 11069-000 Rev. H 3.2 Connecting Power Position the card so its contacts are facing towards the controller and to the left. The label will be facing to ...
https://www.omron.com.tw/data_pdf/mnu/i602-e-03_smartcontroller_ex.pdf
...ions to perform linear interpolation of two axes. The following instructions are created. To do so, we will use axis variables, an axes group, and motion control instructions. Rung 0: Axes Se...
https://www.omron.com.tw/data_pdf/mnu/i827-e1-02_r88m-1(a)__r88d-1s(a)n_-ect.pdf