| IAグローバル検索 |
...fe display function The end of the laser diode lifespan is automatically detected and displayed so maintenance can be performed systematically. On the main digital display of the amplifier, t...
https://www.ia.omron.com/products/family/2979/application.html
...eduction in the need for debugging. Partial adjustments to individual modules is also possible, so assembly and adjustment can be carried out together, which leads to more efficient on-site w...
https://www.ia.omron.com/support/guide/10/further_information.html
...rd configuration, there is no need to set the threshold for monitoring the rotation standstill, so operation can start immediately by connecting the G9SX-SM to the machine. If settings are re...
...11 11 12 20 1 10 2 1 2 3 4 5 6 7 8 9 10 11 CN1 A B C D +24V GND SO RBI LEO1 LEO2 LEO3 TB1 +24V GND ケース SI プリント基板 生産終了商品と推奨代替商品生産終了予定商品形M7E-08DBN2 形M7E-08HBN2...
...RY8 RY7 RY6 RY5 RY4 RY3 RY2 RY1 RY1/a RY2/a RY10/a LED LED G R X Ta 電源回路 Tc X/c Tb F So P1 吸衝収撃回波路 Sa RY10/a RY9/a RY8/a RY7/a RY6/a RY5/a RY4/a RY3/a RY2/a RY1/a T1 T2 T1 T2 T1 T2...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
...ous models from OMRON. The protective structure eliminates the need for screws to hold a cover, so there are no worries about loose screws leading to liquid penetration. And the model number ...
...w beam diameter of minimum 2.5 mm The E3S-DB has a response time of 0.5 ms for a pitch of 5 mm, so detection is possible at a conveyor speed of up to 4 m/s. (With the E3S-DB[][]2(T) and a sen...