| IAグローバル検索 |
... only in place of Service not supported, Attribute not supported and Attribute not settable. 2B-CF --- Reserved by CIP for future extensions D0-FF Reserved for Object Class and service errors...
https://www.omron.com.au/data_pdf/mnu/w536-e1-11_nx-eic202.pdf
...l CFast Card slot and/or an optional Battery are located at the rear side of the base layer. as CF t 3 Additional Information • Refer to 3-6-1 CFast Card Slot (Optional) on page 3-18 for more...
...l CFast Card slot and/or an optional Battery are located at the rear side of the base layer. as CF t 3 Additional Information • Refer to 3-6-1 CFast Card Slot (Optional) on page 3-22 for more...
...yer. The CFast Card slot accepts CFast Cards that comply with the CFast 2.0 specification. t as CF Additional Information Refer to 3-10-4 CFast Cards on page 3-24 for details. 3-18 NY-series ...
https://www.omron.com.au/data_pdf/mnu/w556-e2-08_ny512-1_00.pdf
...r. The CFast Card slot accepts CFast Cards that comply with the CFast 2.0 specification. 3 t as CF Additional Information Refer to 3-10-4 CFast Cards on page 3-27 for details. NY-series Indus...
... only in place of Service not supported, Attribute not supported, or Attribute not settable. 2B-CF D0-FF Reserved by CIP for future extensions. Reserved for Object Class and service errors Th...
https://www.omron.com.au/data_pdf/mnu/w563-e1-08_ny532_ny512.pdf
... only in place of Service not supported, Attribute not supported, or Attribute not settable. 2B-CF D0-FF Reserved by CIP for future extensions. Reserved for Object Class and service errors Th...
https://www.omron.com.au/data_pdf/mnu/w627-e1-05_nx-eip201.pdf
...CFast Card Slot The CFast Card slot is the storage device for the OS and related software. t as CF Additional Information Refer to 3-7-3 CFast Cards on page 3-13 for more information. 3-10 NY...
...FEATURES The following describes the names and functions of parts on the Data Storage Unit. (1) CF power indicator (2) CF access indicator (3) Error indicator (4) Memory Card slot (5...
...E - - RESPONSE RESEND RR - - CONTROLLER CONTROL CC CONTROLLER CONTROL CC READ ERROR INFORMATION CF READ ERROR INFORMATION CF READ HISTORY INFORMATION HI - - Host Commands V680 Comman...
https://www.omron.com.au/data_pdf/mnu/z249-e1-12_v680-ca5d0_-v2.pdf
...ons (1) (2) (3) 1 (4) BEFORE USE (5) (10) (6) (7) (9) (8) (11) (12) (14) (13) Name Function (1) CF power LED Displays the status of the power supplied to the Memory Card. This LED turns ON wh...
https://www.omron.com.au/data_pdf/mnu/z289-e1-03_zg2-dsu.pdf
...cimal symbol None, point (default), or comma Record separator None, comma, tab, space, or CR or CF+LF (default) Use the following menu command to change the output CSV file format. (Setup Mod...
...cimal symbol None, point (default), or comma Record separator None, comma, tab, space, or CR or CF+LF (default) Use the following menu command to change the output CSV file format. (Setup Mod...
https://www.omron.com.au/data_pdf/mnu/z329-e1-02_fq-cr1_____-m.pdf
... the function is disabled DB Indicates that the data type is TIME. When the function is enabled CF Indicates that the data type is DATE AND TIME. ZP-series EtherNet/IP Communication Unit User...
...ibute ID (hex) Data type Event Log 41 00 20 USINT Default (hex) DB Value (Value range) DB: TIME CF: DATE AND TIME ZP-series RS-232C Communication Unit User’s Manual (Z499) A-3 Supported Messa...
...してください。 ・NPN タイプ(形 ZG2-DSU11) 入力 機能 ●図記号の説明 (7)OUT4(BUSY 出力) データをロギング中、またはデータを CF カードに保存中に ONします。 ■入出力段回路図 ■定格 / 性能項目コン...
https://www.omron.com.au/data_pdf/mnu/zg2-dsu___inst-1668182-7c.pdf
...トレートケーブルをご使用ください。 直接パソコンと接続する場合は、LANのクロスケーブルをご使用ください。 個/cf 個/L 各出力端子負荷 + ・ZN-TH11-S接続ポートにはZN-TH11-S以外の機器を接続しないでく...
https://www.omron.com.au/data_pdf/mnu/zn-pd-s_inst-3732738-1j.pdf
...示灯 広レンジ表示灯電源表示灯 メインデジタル表示 リットル表示灯 ① DINレ−ル 押しボタンスイッチ CNT/CF ①、②の順序を逆にしないでください。 逆の順序で装着しますと取り付け強度が低下する場合があ...
https://www.omron.com.au/data_pdf/mnu/zn-pda11_inst-9975423-5e.pdf
...示灯電源表示灯 メインデジタル表示 リットル表示灯 UPキー RIGHTキー LEFTキー ② POWER ×1000 CNT/L ① DINレ−ル CNT/CF ①、②の順序を逆にしないでください。 逆の順序で装着しますと取り付け強度が...
https://www.omron.com.au/data_pdf/mnu/zn-pda12_inst-9978924-1e.pdf
... (4) OUT1 (5) OUT2 (6) OUT3 (7) OUT4 (8) INO (9) IN1 (10) IN2 (11) IN3 (12) 未使用 (6)OUT3(ERR 出力) CF カード書込み / 読込み異常の場合に ONします。 (7)OUT4(BUSY 出力) データをロギング中...
https://www.omron.com.au/data_pdf/mnu/zs-dsu___inst-7934186-4g.pdf