| IAグローバル検索 |
...Precautions -A space of 56mm in diamet- er is needed for rotation. -Model E3S-A can be reverse- ly mounted according to the Note 3 dimensions. Model E3S-A Model E3S-B Model E3R (Typical) [m...
https://www.fa.omron.com.cn/data_pdf/mnu/e39-l97_l98_inst-6918209-1d.pdf
...ed properly. Confirm that the indicators on USB-Infrared Conversion Cable are operating proper- ly. Operating conditions may cause the USB connector, infrared port, or cables to deteriorate f...
https://www.fa.omron.com.cn/data_pdf/mnu/e58-cifir_inst-e.pdf
...with standby sequence) •For the lower-limit alarms in cases 1 and 2 above, the alarm is normal- ly OFF if upper- and lower-limit hysteresis overlaps. •In case 3, the alarm is always OFF. (5) ...
https://www.fa.omron.com.cn/data_pdf/mnu/h157-e1-08_e5cn-h_e5an-h_e5en-h.pdf
...mit is judged to be exceeded during execution of an NC program, each CNC motor stops immediate- ly. In other cases, the path or target position is adjusted so that the software limit is not e...
https://www.fa.omron.com.cn/data_pdf/mnu/o030-e1-07_nj501-5300_ny532-5400.pdf
...he Connector Align the cable connector with the Unit connector, insert the cable connector ful- ly, and tighten the screws on both sides of the connector to lock it in place. Tight- en the sc...
https://www.fa.omron.com.cn/data_pdf/mnu/v066-01_nt-drt21.pdf
...gs. The following con- ditions, however, may prevent sampling from being performed at complete- ly fixed intervals. Be sure to consider possible affects of this on the application in advance....
...ircuiton童herlg抽、8y『θwrit治9thiscode.scantirneissavedandP『og『am rnemoryspacξ≧isL匡sedmore{∋fficien嘘ly. ⑦トe酬⇒ 0209 ...}L-⑤ Theci『cvitoRtheie貴reqし爾esane)(traTernporaryReiayA「ea{TR...
https://www.fa.omron.com.cn/data_pdf/mnu/w131-e1-02_c500.pdf
...imp terminals. Use round crimp terminals for wiring. Do not connect bare stranded wires direct- ly to terminal blocks. Caution Tighten the terminal block screws of the AC Power Supply to a to...
https://www.fa.omron.com.cn/data_pdf/mnu/w136-03_c200h_c500_3g2a6-rm_rt.pdf
...gram Operation Section 2-5 it cannot be written. Press the FUN Key once more and input correct- ly. d) Input the data to be sent. or Note Always press the WRITE Key after inputting the last s...
https://www.fa.omron.com.cn/data_pdf/mnu/w341-e1-05_c200h_cqm1_pro.pdf
...ted by left-click- ing the Cut Icon on the toolbar or by pressing the Ctrl+X Keys. Alternative- ly, right-click to display the pop-up menu and select Cut from the menu. Cut can also be select...
https://www.fa.omron.com.cn/data_pdf/mnu/w344-e1-18_cx-protocol.pdf
...sole is provided with a large display onto which ladder-diagram programs can be written direct- ly in ladder-diagram symbols for input into the PLC without conversion to mne- monic form. hand...
https://www.fa.omron.com.cn/data_pdf/mnu/w367-e1-02_cs1w-slk11_21.pdf
...shown below. Note 1. Be sure to connect the input (24 VDC) for the output power supply correct- ly. 2. Connect loads of between 7 and 30 mA to pulse output. (When connecting loads of less tha...
https://www.fa.omron.com.cn/data_pdf/mnu/w378-e1-02_cs1w-hio_hcp_hca_v1.pdf
...each Slave, as shown in the following diagram, if I/O communications have been started correct- ly. 111 Using DeviceNet Scanner Demo Section 5-2 Note It takes several seconds for a connection...
https://www.fa.omron.com.cn/data_pdf/mnu/w381-e1-03_3g8f7-drm21-e.pdf
...r SPED(64) also) to change the output frequency. The number of output pulses that was previous- ly specified will be output correctly even if the output frequency is changed. The frequency ca...
https://www.fa.omron.com.cn/data_pdf/mnu/w384-e1-01_cs1w-hio01_hcp22_hca22.pdf
... device. OK No Edit Name Changes the selected device’s name. OK No Edit Node Address (slave on- ly) Edits the selected device’s node address. OK No Print Preview Displays the print preview fo...
https://www.fa.omron.com.cn/data_pdf/mnu/w464-e1-15_cx-integrator.pdf
...ount of movement along the path is given by L and amounts of movement of axes 1 and 2 by Lx and Ly, Fx and Fy can be expressed by the formula below: Precautions for Correct Use The status of...
https://www.fa.omron.com.cn/data_pdf/mnu/w477-e1-07_cj1w-nc__4.pdf
...en the device output hold configuration is set to enable. The equipment may operate unexpected- ly because the last status for outputs is retained. •Changing the operating mode of the product...
https://www.fa.omron.com.cn/data_pdf/mnu/w556-e2-08_ny512-1_00.pdf
...re that the terminal blocks, expansion cables, and other items with locking devices are proper- ly locked into place. Installation •Always turn OFF the power supply before installing the Unit...
https://www.fa.omron.com.cn/data_pdf/mnu/w567-e1-09_nx-ilm.pdf
... to each port. AR- RAY[0..1 ]OF BYTE 0000 to FFFF hex Port1 Output Data 01 Yes Ports 1 to 4 on- ly Ports 1 to 8 Port 1 Output Data 02 Same as for Port 1 Output Data 01. AR- RAY[0..1 ]OF BYTE ...
https://www.fa.omron.com.cn/data_pdf/mnu/w570-e1-10_io-link_system.pdf
...er of connections is 10 when tag data links (Class 1), Class 3, and UCMM are used simultaneous- ly. *3. You can configure output retention, clear, and other settings during Idle. Refer to 10-...
https://www.fa.omron.com.cn/data_pdf/mnu/w619-e1-06_nxr-ilm08c-eit.pdf