| IAグローバル検索 |
...输入函数的按钮。 函数说明 SIN(算式) 计算正弦。 结果以-1~1之间的值返回。 算式内指定的角度以[度]为单位指定。 COS(算式) 计算余弦。 结果以-1~1之间的值返回。 算式内指定的角度以[度]为单位指定...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/sdnb-cn5-710a-1_fz4.pdf
...值也分别置为ON。 316 8.可用标准函数可以使用以下C语言的标准函数。 有关详情,请参阅C语言商业手册。 sin (double) cos (double) tan (double) sinh (double) cosh (double) tanh (double) asin (double)...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v106-cn5-24_discon.pdf
...nguage is available. Refer to a commercial handbook of C language for the details. sin (double) cos (double) tan (double) sinh (double) cosh (double) tanh (double) asin (double) acos (double)...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v106-e1-27_nb3q_nb5q_nb7w_nb10w.pdf
...stered in the scan list. A device that is not supported is registered in the scan list (e.g., a COS-only slave). The data size of a device on the network differs from the data size registered...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/v203-e1-03_itnc-eis_eix.pdf
...however this method supports a maxi- mum of 8 bytes of input data from Slaves. change of state (COS) Data is transmitted when the data has changed in the Master or Slave. Data is transmitted ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w347-e1-06_c200hw_cqm1-drt_drt1_delete.pdf
... RECV, and CMND Floating-point Instructions FIX, FIXL, FLT, FLTL, +F,–F, *F, /F, DEG, RAD, SIN, COS, TAN, ASIN, ACOS, ATAN, SQRT, EXP, and LOG The following instructions can be used on the SS...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w363-e1-07_cqm1h.pdf
...tions)•Remote I/O communications (master and slave): Master/slave connection (poll, bit-strobe, COS, cyclic) •Explicit message and FINS message communications: Explicit connection All conform...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w380-e1-10_cs1w_cj1w-drm.pdf
...457 输出需要度→弧度 RAD @RAD 458 输出需要弧度→度 DEG @DEG 459 输出需要正弦 SIN @SIN 460 输出需要余弦 COS @COS 461 输出需要指令助记符代码符号/操作数功能位置执行条件 Md˖㹿Ь佪ᄫ *F(456)...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w394-c1-07_cj_cs_discon.pdf
...s No 2nd Term Within the opera- tion numerical value range Yes Yes Read No Yes No Yes No Cosine COS #MF- = COS#MF-; 1st Term --- No No Write No Yes No Yes No 2nd Term Within the oper...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w419-e1-04_cs1w_mch.pdf
... 459 S:第一个源字REAL --- R:第一个结果字REAL --- SINE SIN @SIN 460 S:第一个源字REAL --- R:第一个结果字REAL --- COSINE COS @COS 461 S:第一个源字REAL --- R:第一个结果字REAL --- TANGENT...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w447-cn5-02_cx-programmer_discon.pdf
... 459 S:第一个源字REAL --- R:第一个结果字REAL --- SINE SIN @SIN 460 S:第一个源字REAL --- R:第一个结果字REAL --- COSINE COS @COS 461 S:第一个源字REAL --- R:第一个结果字REAL --- TANGENT...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w447-cn5-03_discon.pdf
...tup Button, click the Connection Tab, and select User Setup. Select Use Poll Connection and Use COS Connection and then select output data, input data, and generic status for the respective c...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w454-e1-04_grt1-drt.pdf
... with Terminal Block (Independent Relays) Model CJ1W-OC201 Max. Switching Capacity 2 A 250 VAC (cos= 1), 2 A 250 VAC (cos= 0.4), 2 A 24 VDC (16 A/Unit) Min. Switching Capacity 1 mA...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w472-e1-17_cj2h-cpu6_eip_cj2m-cpu.pdf
...度→弧度RAD @RAD 458输出需要弧度→度DEG @DEG 459输出需要正弦SIN @SIN 460输出需要高速正弦SINQ @SINQ 475输出需要余弦COS @COS 461输出需要高速余弦COSQ @COSQ 476输出需要正切TAN @TAN 462输出...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/w473-cn5-09_discon.pdf
...cannot be continued if it was modified while execution was stopped. CONT Reference Section 5 77 COS COSine (Function) Action Determines the cosine of an angle. Format COS (numeric ex...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z109-02a_f350.pdf
...le0 ENT:Select Position Measurement Variable Data Judge Constant ← ABS MOD MAX MIN SQRT DEL SIN COS ANGL ATAN DIST BS AND OR NOT OK Variable0 ENT:Select Position Measurement Variable Data Jud...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z147-e1-02_f160.pdf
...le0 ENT:Select Position Measurement Variable Data Judge Constant ← ABS MOD MAX MIN SQRT DEL SIN COS ANGL ATAN DIST BS AND OR NOT OK Variable0 ENT:Select Position Measurement Variable Data Jud...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z173-e1-02b_f160-2.pdf
...power supply and load. OUT0 OUT1 OUT2 OUT3 Expansion I/O Unit Load Load Load Load 250 VAC, 8 A (cos f = 1) 24 VDC, 5 A Q0 +− Q1 Q2 Q3 +−+−+− CPU Unit with 10 I/O points Load Load Load Load Lo...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z183-e1-01a_zen.pdf
...he range of -1 to 1. Indicate s the angle designate d in the numerica l expressio n in degrees. COS (equation) Calculate s the cosine . The result will be returned within the range of -1 to 1...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z291-e1-05_fz3.pdf
...e. The result is a value between−1 and 1. The angle in the expression is in degrees. SIN(angle) COS Finds the cosine. The result is a value between−1 and 1. The angle in the expression is in ...
https://www.fa.omron.com.cn/data_pdf/closed/mnu/z302-e1-03a_fq.pdf