Page top

Sysmac Studio Ver.1.[][]

Automation Software Sysmac Studio

Sysmac Studio Ver.1.[][]

Provides an integrated development environment for NJ/NX/NY-series Controllers. With its intuitive user interface, integrates programming, test and debug of logic, motion, safety and vision sensors and achieves an advanced security function.

License portal

License portal: Get an installer and free trial license, view license usage, and transfer licenses.

Automation Software

A license is required to use Sysmac Studio. There are two types of licenses: Network Licenses for the 64-bit application and Standalone Licenses for the 32-bit application.
The installer for the Sysmac Studio 64-bit application is available on the website, License Portal. If you want an installer DVD for the Sysmac Studio 32-bit or 64-bit application, please purchase the Sysmac Studio DVD.

Network Licenses (64-bit application only)

Sign up as a user on the License Portal site and download the installer image file after purchasing a new Network License. For more information,
visit this site: https://license-user.automation.omron.com/.

Product name Specifications Model
Number of
licenses
Sysmac Studio
Basic License
Sysmac Studio is an integrated development environment for
configuring, programming, debugging, and maintaining our
machine automation controllers including the NJ/NX-series CPU
Units and the NY-series Industrial PCs, EtherCAT Slave Units,
and HMIs.
1 license SYSMAC-BA201L
Sysmac Studio
Advanced License
This license allows you to use the 3D Simulation Option and the
Team Development Option in addition to the functions covered
by the Basic License.
1 license SYSMAC-AD201L
Sysmac Studio
Upgrade License
for Advanced
This license upgrades your Basic License to the Advanced
License.
1 license SYSMAC-AD501L

Standalone Licenses

If you use the Sysmac Studio 32-bit application, purchase a Standalone License. We recommend a Network License for customers using the Sysmac Studio 64-bit application.

Product name Specifications Model
Number of
licenses
Sysmac Studio
Standard Edition
Ver.1.[][]
Sysmac Studio is the software that provides an integrated
development environment: setting, programming, debugging and
maintenance for Machine Automation Controllers (NJ/NX-series
CPU Units, NY-series Industrial PC), EtherCAT Slaves, and HMIs.
1 license SYSMAC-SE201L
3 licenses SYSMAC-SE203L
10 licenses SYSMAC-SE210L
30 licenses SYSMAC-SE230L
50 licenses SYSMAC-SE250L
Sysmac Studio
Vision Edition
Ver.1.[][]
Sysmac Studio Vision Edition is the license providing only the
necessary functions for settings of FH, FHV7 and FQ-M Series
Vision Sensors. This edition is valid for FH, FHV7 and FQ-M
Series Vision Sensors only.
1 license SYSMAC-VE001L
Sysmac Studio
Measurement
Sensor Edition
Ver.1.[][]
Sysmac Studio Measurement Sensor Edition is the license
providing only the necessary functions for settings of ZW-series
Measurement Sensors. This edition is valid for ZW-series
Measurement Sensors only.
1 license SYSMAC-ME001L
3 licenses SYSMAC-ME003L
Sysmac Studio
NX-I/O Edition
Ver.1.[][]
Sysmac Studio NX-IO Edition is the license providing only the
necessary functions for settings of couplers for EtherNet/IP and
PROFINET. This edition is valid for couplers of EtherNet/IP and
PROFINET only.
1 license SYSMAC-NE001L
Sysmac Studio
Drive Edition
Ver.1.[][]
Sysmac Studio Drive Edition is the license providing only the
necessary functions for settings of drive units. This edition is valid
for 1S/ G5-series units only.
1 license SYSMAC-DE001L
Sysmac Studio
Safety Edition
Ver.1.[][]
Sysmac Studio Safety Edition is the license providing only the
necessary functions for settings of a safety control system. This
edition is valid for communication controllers and EtherNet/IP
couplers only.
1 license SYSMAC-FE001L

Optional Licenses for Standalone Licenses

These products are applicable to Sysmac Studio Standard Edition only.
Optional licenses cannot be applied to network licenses.

Product name Specifications Model
Number of
licenses
Sysmac Studio
Team
Development
Option
Sysmac Studio Team Development Option is the
license to enable the project version control functionality.
1 license SYSMAC-TA401L
3 licenses SYSMAC-TA403L
10 licenses SYSMAC-TA410L
30 licenses SYSMAC-TA430L
50 licenses SYSMAC-TA450L
Sysmac Studio
3D Simulation
Option
Sysmac Studio 3D Simulation Option is the license to
enable the 3D Simulation functionality.
The option is valid for the 64-bit Sysmac Studio only.
1 license SYSMAC-SA401L-64
3 licenses SYSMAC-SA403L-64
10 licenses SYSMAC-SA410L-64
30 licenses SYSMAC-SA430L-64
50 licenses SYSMAC-SA450L-64

Sysmac Studio DVD

License keys are not included. Licenses are required listed above.

Product name Specifications Model
Supporting OS Number of licenses
Sysmac Studio
Ver.1.[][]
32-bit DVD
Windows 7 (32/64-bit)/8.1 (32/64-bit)/
10 (32/64-bit)/11 (64-bit)
-
(Installation media only.
A license of each edition
is required.)
SYSMAC-SE200D
Sysmac Studio
Ver.1.[][]
64-bit DVD
Windows 10 (64-bit)/11 (64-bit) SYSMAC-SE200D-64

Note: You can also download the installer image file for installation by signing up as a user on the License Portal site.
         For more information, visit this site: https://license-user.automation.omron.com/.

Components

DVD (SYSMAC-SE200D/SYSMAC-SE200D-64)

Components Details
Introduction An introduction about components, installation/uninstallation, user registration and auto
update of the Sysmac Studio is provided.
Setup disk (DVD-ROM) 1

License (SYSMAC-BA2[][]L/AD2[][]L/AD5[][]L/SE2[][]L/VE0[][]L/ME0[][]L/NE0[][]L/DE0[][]L/TA4[][]L/FE0[][]L/SA4[][]L-64)

Components Details
License agreement The license agreement gives the usage conditions and warranty for the Sysmac Studio.
License card A model number, version, license number, and number of licenses are described.
User registration card *1 Two cards are contained. One is for users in Japan and the other is for users in other
countries.

*1. Not come with SYSMAC-BA2[][]L, AD2[][]L, and AD5[][]L.

Included Support Software

DVD media of Sysmac Studio includes the following support software.

Included Support Software Outline
CX-Designer Ver.3.[] The CX-Designer is used to create screens for NS-series PTs. *1
CX-Integrator Ver.2.[] The CX-Integrator is used to set up FA networks.
CX-Protocol Ver.2.[] The CX-Protocol is used for protocol macros for Serial Communications Units.
Network Configurator Ver.3.[] The Network Configurator is used for tag data links on the built-in EtherNet/IP port.
SECS/GEM
Configurator
Ver.1.[] The SECS/GEM Configurator is used for SECS/GEM settings.
Adept Robot IP
Address Setting Tool
Ver.1.[] The Adept Robot IP Address Setting Tool is used for setting IP address of Adept Robot.
CX-ConfiguratorFDT Ver.3.[] The software that sets the IO-Link devices.
IODD DTM
Configurator
Ver.3.[] The software that adds and deletes IODD files for the IO-Link devices.

*1. Please use the Sysmac Studio to create the project of the NA Series.