Page top

CS1D

CS1D Overview

CS1D

Redundant CPU Units, Power Supply Units, Communications Units, and Expansion I/O Cables

With the CS1D, you can select from a variety of redundant systems.

In addition to duplexed CPU Units and Power Supply Units, the customer can duplex other components, such as Communications Units (Controller Link or Ethernet) and Expansion Cables, to match the system requirements and provide a diverse range of duplex system configurations.

The CS1D supports a variety of network configurations.

Ethernet can be duplexed as well as Controller Link, which both have a proven track record in FA applications.
In addition, a variety of networks are available for lower-level I/O, including DeviceNet, CompoNet, and the MECHATROLINK-II Motion Controller network. Both DeviceNet and CompoNet are open networks that boast a proven track record with the CS1 Series.

With the CS1D, a highly reliable system can be introduced easily.

Of course, the standard CS-series PLC resources can be used as-is, and a CS1D Duplex System can be set up and used easily, even by users setting up a duplex system for the first time.

CS1D Features 7 CS1D_Features1

In OMRON's proprietary hot-standby method, all data is shared simultaneously.

If an error occurs in the active CPU Unit, a switching program is not needed in the standby CPU Unit!

CPU Unit operation switches smoothly. Switching time is short, so operation can continue without bumps.

CS1D Features 11 CS1D_Features2
CS1D Features 12 CS1D_Features3
CS1D Features 13 CS1D_Features4

Since the active and standby CPU Units always operate synchronously, control continues automatically and continuously in the standby CPU Unit if an error occurs in the active CPU Unit.

CS1D Features 15 CS1D_Features5
CS1D Features 16 CS1D_Features6

The standby CPU Unit is normally stopped. If an error occurs in the active CPU Unit, the standby CPU Unit becomes the active CPU Unit. The transfer between CPU Units is limited and control is discontinuous due to initialization during the switch-over.

CS1D Features 18 CS1D_Features7

The CPU Unit automatically selects the normally functioning Communications Unit.

When an error occurs, it is not necessary to use a complex switching program or special data link area for duplexing!

CS1D Features 21 CS1D_Features8

When Ethernet Units are used, complex switching programs for message communications can be simplified.

Typical duplex program

CS1D Features 24 CS1D_Features9

OMRON duplex program

CS1D Features 26 CS1D_Features10

When using a Controller Link Unit, data link area allocations can be configured without waste.

Typical duplex program

CS1D Features 29 CS1D_Features11

OMRON duplex program

CS1D Features 31 CS1D_Features12

New Release! The Ultimate Duplex "Dual I/O Expansion" System

The newly released Duplex CPU, Dual I/O Expansion system draws attention in the maintenance field! This system answers the needs of users who want to make improvements and add functions without stopping the equipment. This strengthens the proven CS1D Duplex System even more.

Note:The functions in this section are supported only in a Duplex CPU, Dual I/O Expansion System.

CS1D Features 35 CS1D_Features13

Special Programming Devices and Displays are not required for Online Unit Replacement.

A computer is not needed for onsite operations!

Units can be replaced without knowing Programming Device procedures!

CS1D Features 39 CS1D_Features14

Units and Expansion Backplanes can be added online.

Functions can be added easily after the system has started operating, even if the system cannot be turned OFF or stopped.

Adjustments and improvements can be easily made when setting up new systems without turning OFF the power.

While online, a Unit can be added easily to an empty slot. (This function is supported in Duplex CPU Single I/O Expansion Systems and Duplex CPU Dual I/O Expansion Systems.)

CS1D Features 44 CS1D_Features15

In addition, an Expansion Backplane as well as its mounted Units can be added easily.

CS1D Features 46 CS1D_Features16
CS1D Features 47 CS1D_Features17

Expansion Cables can be duplexed and Units can be replaced Online.

By duplexing the Expansion Units and Expansion Cables, the Expansion Cables are duplexed and can be replaced during operation. In addition, cable disconnections are monitored so failures can be located easily.

CS1D Features 50 CS1D_Features18

Duplex Units can be replaced online.

CS1D Features 52 CS1D_Features19

PLC-based Process Control System for Full-scale Process Control

CS1D Features 54 CS1D_Features20

A variety of system configurations can be created, such as a Duplex CPU System using a CS1D Process-control CPU Unit with a built-in Loop Control Board (LCB) function or a Single CPU System using a Loop Control Board mounted in the CS1D CPU Unit's Inner Board slot. You can retain the openness and cost performance of a general-purpose PLC base while expanding the possible range of PLC control with process control functions and reliability that are equivalent to some of the functions and performance of DCS.

CS1D Features 56 CS1D_Features21
CS1D Features 57 CS1D_Features22

Previous System Issues

Initial costs are high because a large-scale system must be used.

CS1D Features 60 CS1D_Features23

PLC-based Process Control Solution

[Down-sizing]
Using the PLC base saves cost, space, and time.

CS1D Features 63 CS1D_Features24