Page top

NJ501-[][][][]

NJ-Series NJ501 CPU Units

NJ501-[][][][]

New controller that covers functions and high-speed processing required for machine control and safety, reliability and maintainability that are the features of industrial controllers. Ideal for large-scale, fast, and high-accurate control with up to 64 axes.

• Integration of Logic and Motion in one CPU.

• Conforms to IEC 61131-3 (JIS B 3503) standard programming and PLCopen function blocks for Motion Control.

 Programming with variables allows users to create complex programs efficiently.

• Fast and accurate control by synchronizing all EtherCAT devices, such as vision sensors, servo drives, and field devices, with the PLC and Motion Engines.

• Offers speed without compromising on reliability and robustness expected from PLCs.

• Complete RAS functions: Transmission frame error check, timeout, bus diagnosis, Watchdog (WDT), memory check, and topology check, etc.

• Ideal for large-scale, fast, and high-accurate control with up to 64 axes.

• Linear and circular interpolation.

• Electronic gear and cam synchronization.

• The Controller can be directly connected to a database. No special Unit, software, nor middleware is required. (NJ501-[][]20)

Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
Microsoft, Windows, Windows Vista and SQL Server are registered trademarks of Microsoft Corporation in the United States and other countries.
Oracle and Oracle Database are trademarks or registered trademarks of Oracle Corporation and/or its affiliates in the United States and other countries.
IBM and DB2 are trademarks or registered trademarks of International Business Machines Corp., registered in the United States and other countries.
SEMI® is a trademark or registered trademark of Semiconductor Equipment and Materials International in the United States and other countries.
EtherCAT® is a registered trademark of Beckhoff Automation GmbH for their patented technology.
EtherNet/IPTM, DeviceNetTM are trademarks of the ODVA.
Other company names and product names in this document are the trademarks or registered trademarks of there respective companies.