Page top

SYSMAC-SE2[][][]

Automation Software Sysmac Studio

SYSMAC-SE2[][][]

Provides an integrated development environment for NJ/NX/NY-series Controllers. With its intuitive user interface, integrates programming, test and debug of logic, motion, safety and vision sensors and achieves an advanced security function.

Automation Software

Please purchase a DVD and licenses the first time you purchase the Sysmac Studio. DVDs and licenses are available individually.
The license does not include the DVD.

Sysmac Studio DVD

License keys are not included. License keys of each Sysmac Studio edition (and a license keys of options, if necessary) are required.

Product name Specifications Model
Supporting OS Number of
licenses
Sysmac Studio
Ver.1.[][]
32-bit DVD
Windows 7 (32/64-bit)/8 (32/64-bit)/
8.1 (32/64-bit)/10 (32/64-bit)
-
(Installation media only.
A license of each
edition is required.)
SYSMAC-SE200D
Sysmac Studio
Ver.1.[][]
64-bit DVD
Windows 10 (64-bit) SYSMAC-SE200D-64

Licenses for Sysmac Studio Editions

License key only. The Sysmac Studio DVD is necessary.

Product name Specifications Model
Number of
licenses
Sysmac Studio
Standard Edition
Ver.1.[][] *1
Sysmac Studio is the software that provides an integrated
development environment: setting, programming, debugging and
maintenance for Machine Automation Controllers (NJ/NX-series
CPU Units, NY-series Industrial PC), EtherCAT Slaves, and HMIs.
1 license SYSMAC-SE201L
3 licenses SYSMAC-SE203L
10 licenses SYSMAC-SE210L
30 licenses SYSMAC-SE230L
50 licenses SYSMAC-SE250L
Sysmac Studio
Vision Edition
Ver.1.[][]
Sysmac Studio Vision Edition is the license providing only the
necessary functions for settings of FQ-M and FH-series Vision
Sensors. This edition is valid for FQ-M and FH-series Vision
Sensors only.
1 license SYSMAC-VE001L
Sysmac Studio
Measurement
Sensor Edition
Ver.1.[][]
Sysmac Studio Measurement Sensor Edition is the license
providing only the necessary functions for settings of ZW-series
Measurement Sensors. This edition is valid for ZW-series
Measurement Sensors only.
1 license SYSMAC-ME001L
3 licenses SYSMAC-ME003L
Sysmac Studio
NX-I/O Edition
Ver.1.[][]
Sysmac Studio NX-IO Edition is the license providing only the
necessary functions for settings of EtherNet/IP couplers. This
edition is valid for EtherNet/IP couplers only
1 license SYSMAC-NE001L
Sysmac Studio
Drive Edition
Ver.1.[][]
Sysmac Studio Drive Edition is the license providing only the
necessary functions for settings of drive units. This edition is valid
for 1S/ G5-series units only.
1 license SYSMAC-DE001L
Sysmac Studio
Safety Edition
Ver.1.[][]
Sysmac Studio Safety Edition is the license providing only the
necessary functions for settings of a safety control system. This
edition is valid for communication controllers and EtherNet/IP
couplers only.
1 license SYSMAC-FE001L

*1. We offer Site Licenses for users who will run Sysmac Studio on multiple computers. Ask your OMRON sales representative for details.

Licenses for Sysmac Studio Options

These products are applicable to Sysmac Studio Standard Edition only.

Product name Specifications Model
Number of
licenses
Sysmac Studio
Team
Development
Option
Sysmac Studio Team Development Option is the
license to enable the project version control functionality.
1 license SYSMAC-TA401L
3 licenses SYSMAC-TA403L
10 licenses SYSMAC-TA410L
30 licenses SYSMAC-TA430L
50 licenses SYSMAC-TA450L
Sysmac Studio
3D Simulation
Option
Sysmac Studio 3D Simulation Option is the license to
enable the 3D Simulation functionality.
The option is valid for the 64-bit Sysmac Studio only.
1 license SYSMAC-SA401L-64
3 licenses SYSMAC-SA403L-64
10 licenses SYSMAC-SA410L-64
30 licenses SYSMAC-SA430L-64
50 licenses SYSMAC-SA450L-64

Note: We offer Site Licenses for users who will run Sysmac Studio on multiple computers. Ask your OMRON sales representative for details.

Components

DVD (SYSMAC-SE200D)

Components Details
Introduction An introduction about components, installation/uninstallation, user registration and auto
update of the Sysmac Studio is provided.
Setup disk (DVD-ROM) 1

License (SYSMAC-SE2[][]L/VE0[][]L/ME0[][]L/NE0[][]L/DE0[][]L/RA4[][]L/TA4[][]L/FE0[][]L/SA4[][]L-64)

Components Details
License agreement The license agreement gives the usage conditions and warranty for the Sysmac Studio.
License card A model number, version, license number, and number of licenses are described.
User registration card Two cards are contained. One is for users in Japan and the other is for users in other
countries.

Included Support Software

DVD media of Sysmac Studio includes the following support software.

Included Support Software Outline
CX-Designer Ver.3.[] The CX-Designer is used to create screens for NS-series PTs. *1
CX-Integrator Ver.2.[] The CX-Integrator is used to set up FA networks.
CX-Protocol Ver.1.[] The CX-Protocol is used for protocol macros for Serial Communications Units.
Network Configurator Ver.3.[] The Network Configurator is used for tag data links on the built-in EtherNet/IP port.
SECS/GEM
Configurator *2
Ver.1.[] The SECS/GEM Configurator is used for SECS/GEM settings.
Adept Robot IP
Address Setting Tool
Ver.1.[] The Adept Robot IP Address Setting Tool is used for setting IP address of Adept Robot.
CX-ConfiguratorFDT Ver.2.[] The software that sets the IO-Link devices.
IODD DTM
Configurator
Ver.3.[] The software that adds and deletes IODD files for the IO-Link devices.

*1. Please use the Sysmac Studio to create the project of the NA Series.
*2. Please purchase the required number of SECS/GEM Configurator licenses.