![]()
Global
These are navigation links to move inside this page.
Rotary Encoders measure the number of rotations, the rotational angle, and the rotational position. Linear Encoders are also available to measure linear movement.
|
|
|
|
|
|
| Engineering Data |
|
![]()
Interpreting Engineering Data
| Bearing Life | Cable Extension Characteristics |
| E6B2-C | E6B2-CWZ6C |
![]() | ![]() |
| Measurement Example Power supply voltage: 5 VDC Load resistance: 1 kΩ (Output residual voltage is measured at a 35 mA load current.) Cable: Special Cable | |
| ・ This graph shows the relationship between mechanical life and the load applied to the shaft. ・ The size of the load during rotation affects the life of the bearings. | ・ This graph shows the effect of the output waveform if the cable is extended. ・ Extending the cable length not only changes the startup time, but also increases the output residual voltage. |