Page top

Lead Contents

Signal Converters

Introduction Features
Principles Classifications
Engineering Data Further Information
Explanation of Terms Troubleshooting

Related Contents

Primary Contents



What Is a Signal Converter?

A Signal Converter is a device that converts signals from sensors to industrial current signals, converts analog input signals to analog output signals, normalizes signals, or isolates signals.
The electronic signals that are detected by a detector are different in nature because of differences in the data that was measured (e.g., temperatures, pressures, and voltages). This makes it difficult to input the data directly into control circuits. Therefore, it is necessary to covert or normalize the data to a signal form that is easy to use.

Types and Functions of Converters

Types of Converter

Signal convertersIsolators
Sensor input converters
Distributors
Alarms
Pulse I/O converters
Characteristic converters
Interface converters

Main Functions

Signal Converters

Converts a DC current/voltage input to a DC voltage/current and outputs the result.

Isolates the input signal and outputs the signal.

Converts the input signal from a thermocouple to a current/voltage and outputs the result.

Converts the signal from a load cell to a voltage/current and outputs the result.

Converts the rate of input pulses and outputs the result.

Converts a pulse signal to an analog signal and outputs the result.

Converts an analog signal to a pulse signal and outputs the result.

Linearizes a signal that does not have linear output characteristics and outputs the result.

Interface Converters

Converts between RS-232C/USB and RS-422/485 serial protocols.

Classifications

OMRON Converters are classified as shown below.

Configuration Examples for Major Converters

Signal Converters

Isolators

The effects of problems in the field can be minimized by electrically isolating control equipment in a control room from problems that are caused by the environment in the field.

Thermocouple Converters

The temperature in a gas-fired furnace is measured with a thermocouple and converted to a normalized DC signal by passing it through a thermocouple converter, and then that signal is input into the controller. The controller can control the temperature inside the furnace by comparing the temperature to the set value and controlling a valve.

Pulse Converters

Rotary speed control can be performed by converting a rotary pulse signal from a proximity sensor to an analog signal.

Load Cell Converters

The measurement results from a load cell can be digitally displayed on a digital panel indicator.Using the digital panel indicator’s functions, an alarm can also be output for a set threshold, in addition to displaying the measurement results.