The following symbols are used to ensure proper product operation.
| Symbol | Meaning | |
|---|---|---|
| New products | ||
| International Standards | UL(See note.) | |
| UL(CSA) (See note.) | ||
| CSA | ||
| VDE | ||
| TÜV | ||
| EU Directives | ||
| Certified for Chinese Standards | ||
Warnings in Precautions and Safety Precautions are indicated as shown in the following table.
| Classification | Symbol | Meaning | |
|---|---|---|---|
| Ite m s for product safety | Precautionary information | Indicates an imminently hazardous situation which, if not avoided, is likely to result in serious injury or may result in death. Additionally there may be severe property damage. | |
| Indicates a potentially hazardous situation which, if not avoided, will result in minor or moderate injury, or may result in serious injury or death. Additionally there may be significant property damage. | |||
| Indicates a potentially hazardous situation which, if not avoided, may result in minor or moderate injury or in property damage. | |||
| Points to note | Precautions for Correct Use | Supplementary comments on what to do or avoid doing, to prevent failure to operate, malfunction or undesirable effect on product performance. | |
| Other items | Precautions for Safe Use | Supplementary comments on what to do or avoid doing, to use the product safely. | |
| Symbol | Meaning | |
|---|---|---|
| Precautionary information | General Caution Indicates general cautionary, warning, or danger level information |
|
| Explosion Caution Indicates the possibility of explosion under specific conditions |
||
| Electrical Shock Caution Indicates possibility of electric shock under specific conditions |
||
| High Temperature Caution Indicates the possibility of injury by high temperature under specific conditions |
||
| Laser Caution Indicates information related to laser safety |
||
| Prohibitions | General Prohibition Indicates a general prohibition |
|
| Contact Prohibition Indicates prohibition of coming into contact with a specific part of a specific device under specific condition because of the possibility of injury. |
||
| Disassembly Prohibition Indicates that disassembly is prohibited to prevent electric shock. |
||
| Mandatory actions | General Mandatory Action Indicates a general action that must be performed by the user. |
|
| Mandatory Ground Indicates that a ground that must be connected by the ser for a device equipped with a ground terminal. |
||
| Nickel-Cadmium Battery Collection Indicates a nickel-cadmium battery that must be collected and recycled. |
||
In line with international standards, this catalog uses SI units. Some conversions from units that have been used in our previous catalogs to SI units are given in the following table.
SI unit Conversions (
Units in shaded boxes are SI units.)
| m/s2 | G |
| 1 | 1.01972x10-1 |
| 9.80665 | 1 |
| N | kgf |
| 1 | 1.01972x10-1 |
| 9.80665 | 1 |
| N • m | kgf • cm | kgf • m |
| 1 | 1.01972x10 | 1.01972x10-1 |
| 9.80665x10-2 | 1 | 1x10-2 |
| 9.80665 | 1x102 | 1 |
| Pa | kPa | kgf/cm2 | mmHg(Torr) | mmH2O |
| 1 | 1x10-3 | 1.01972x10-5 | 7.50062x10-3 | 1.01972x10-1 |
| 1x103 | 1 | 1.01972x10-2 | 7.50062 | 1.01972x102 |
| 9.80665x104 | 9.80665x10 | 1 | 7.35559x102 | 1x104 |
| 1.33322x102 | 1.33322x10-1 | 1.35951x10-3 | 1 | 1.35951x10 |