... axis adjustment. • High stability with unique algorithm that prevents interference of external light. • Models are available with Laser type and IO-Link type. • UL certification (UL60947-5-2...
... last update: April 19, 2017 • Series includes models that enable switching between dark-ON and light-ON operation. • Response frequency as high as 1 kHz. • Easy operation monitoring with bri...
...y adjustment with a built-in sensitivity adjuster. • Easy optical axis monitoring with a bright light indicator. • Compact design incorporating a built-in amplifier and special IC enables dir...
...screw terminal sockets by combining with push-in plus terminal sockets (PYF-[]-PU) that feature light insertion force and strong pull-out strength to achieve less wiring work. • In addition t...
...screw terminal sockets by combining with push-in plus terminal sockets (PTF-[]-PU) that feature light insertion force and strong pull-out strength to achieve less wiring work. • The standard ...
...afety Sensor enters the interlock state, it keeps the control outputs in the OFF state. Even if light becomes incident for all the beams, the control outputs will not go to the ON state. If n...
...afety Sensor enters the interlock state, it keeps the control outputs in the OFF state. Even if light becomes incident for all the beams, the control outputs will not go to the ON state. If n...
...afety Sensor enters the interlock state, it keeps the control outputs in the OFF state. Even if light becomes incident for all the beams, the control outputs will not go to the ON state. If n...
... Input A Photoelectric Sensor is an input device that detects an object when that object blocks light. Each time the light is blocked, the Photoelectric Sensor sends a signal to the ...