Primary Contents

Site Search Results

Site Search Product Search
Results 21 - 30 of 40
G - Solid-state Relays - Item A to Z Index | OMRON...
...olid-state Relays is a product of less than 18. G32A-B G32A-C G32A-D G3F / G3FD G3FM G3H / G3HD G3NA G3NE G3PE (Single-phase) G3PE (Three-phase) G3PF G3PH G3PJ G3R-I/O G3RV-ST G3RZ G3TA G9H...

https://www.ia.omron.com/products/index/relays/solid-state-relays/G.html

faq02041
... Contents Question What is the difference between phototriac and photocoupler isolation for the G3NA Solid-state Relay? Answer  The applicable output load voltage range is different. Solid-s...

https://www.ia.omron.com/support/faq/answer/18/faq02041/

faq02044
...he case for Solid-state Relays with DC inputs that use a constant current input method (such as G3NA and G3PA). Ratings Applicable model Item Rated voltage Operating voltage Impedance Model ○...

https://www.ia.omron.com/support/faq/answer/18/faq02044/

FAQ02075 for Solid-state Relays | OMRON Industrial...
...ll damage the output elements. 2.The following models have a built-in surge-absorbing varistor: G3NA, G3S, G3PA, G3PB, G3NE, G3J, G3NH, G9H, G3DZ (some models), G3RZ, G3FM 3.Be sure to take m...

https://www.ia.omron.com/support/faq/answer/18/faq02075/

faq02235
...Output-ON voltage drop (V) x Carry current (A) For example, if a load current of 8 A flows from G3NA-210B Solid-state Relays, the following heating value will be obtained. P = 1.6 V x 8 A = 1...

https://www.ia.omron.com/support/faq/answer/18/faq02235/

faq03202
...t product (See note 1.) Note Model number 5 A G3N-205BM DC3-30 None See note 2. G3N-205B DC4-30 G3NA-205B DC5-24 See note 3. G3N-205B AC75-125 G3NA-205B AC100-120 G3N-205B AC150-250 ...

https://www.ia.omron.com/support/faq/answer/18/faq03202/

Further Information of Temperature Controllers | O...
... SSRs can be connected. *4. One G3PA-BL SSR can be connected. *5. Two of the -UTU models of the G3NA SSRs can be connected. *6. One of the -UTU model of the G3NA SSRs can be connecte...

https://www.ia.omron.com/support/guide/53/further_information.html

Relays - UL Certification - Americas, US and Canad...
...SL-US --- UL508 NMFT2 Recognized 2A 250V AC G3TA-ODX02S-US --- UL508 NMFT2 Recognized 2A 60V DC G3NA-205B(-UTU) --- UL508 NMFT2, NMFT8 Recognized 5A 240V AC G3NA-210B(-UTU) --- UL508...

https://www.ia.omron.com/support/models/ul/relay.html

Safety Precautions of Solid-state Relays Cautions ...
...der resistance, use the following formula. For SSRs with constant-current input circuits (e.g., G3NA, G3PA, G3PE, G3PJ), calculation is performed at 0.1 mA. 3. ON/OFF Frequency An SSR has del...

https://www.ia.omron.com/product/cautions/18/safety_precautions.html

Further Information of Solid-state Relays | OMRON ...
...ance R must be determined according to the surge withstand current of the SSR. For example, the G3NA-220B-UTU withstands an surge current of 220 A. The value of the protective resistance R is...

https://www.ia.omron.com/support/guide/18/further_information.html

Results 21 - 30 of 40