... of coaxial cables or shielded cables for Photoelectric Sensors and Proximity Sensors? Answer A minimum bending radius of five times cables diameter is recommended for coaxial cables and sh...
...s can be connected if power is supplied to both sides of the B7AP-S1 and B7AP-M1. In this case, a 2-wire AC Sensor or Programmable Controllers can also be connected. Power and Transmission Si...
...tents FAQ No. FAQ00316 Related Contents Primary Contents Question What's the difference between a Reflective Fiber Unit and a Coaxial Reflective Fiber Unit? Answer The sensing surf...
...e do to resolve it? Answer It's possible that the malfunction is due to electrical noise. Try a countermeasure for noise. Different countermeasures should be used depending on factors such ...
...oelectric Sensors Lead Contents FAQ No. FAQ00408 Related Contents Primary Contents Question Can a Photoelectric Sensor with an Optical Fiber be used in an explosion-proof area? Answer Every...
...+99°C -9.9 to +9.9°C Input shift display L99 to H99 L9.9 to H9.9 Applicable Models: E5CS K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Si...
...ers Lead Contents FAQ No. FAQ00564 Related Contents Primary Contents Question There seems to be a large error in the temperature of the Temperature Controller. Why is this? Answer The follo...
...ermom- eter The electrical resistance of the metal used by platinum resistance thermometers has a fixed relationship to the temperature. Therefore, a platinum wire with extremely hig...
... production equipment The Omron HMI enables faster, more efficient control and monitoring - and a more natural, proactive relationship between operator and machine. Vision sensors for high-sp...
...o Multivendor Controller Networks CJ-series DeviceNet Unit CJ1W-DRM21 Smallest in the Industry! A DeviceNet Unit for the CJ Series that Boasts Industry-leading Performance and Functions...