...al Automation voltage reduction unit Definition The appropriate product category Push Buttons / Indicator Lamps A lighting unit that has a smoothing circuit and resistor. The unit lights the ...
...ndustrial Automation forward current Definition The appropriate product category Push Buttons / Indicator Lamps The current that flows to the LED....
...Industrial Automation contact rating Definition The appropriate product category Push Buttons / Indicator Lamps The rated voltage and current that can be applied to the contacts....
...N Industrial Automation set position Definition The appropriate product category Push Buttons / Indicator Lamps The position of an alternate action pushbutton when it is in the self-held stat...
...ustrial Automation number of notches Definition The appropriate product category Push Buttons / Indicator Lamps The number of positions or number of state changes that the selector or key can...
...dustrial Automation releasing travel Definition The appropriate product category Push Buttons / Indicator Lamps The distance or angle through which the pushbutton moves in going from the retu...
...trial Automation push-pull operation Definition The appropriate product category Push Buttons / Indicator Lamps An operation in which an internal mechanical lock mechanism holds the pushbutto...
...ial Automation push-lock, turn-reset Definition The appropriate product category Push Buttons / Indicator Lamps An operation in which an internal mechanical lock mechanism holds the pushbutto...
...ndustrial Automation matrix mounting Definition The appropriate product category Push Buttons / Indicator Lamps A method in which more than one Switch is mounted side-by-side horizontally or ...
...dustrial Automation momentary action Definition The appropriate product category Push Buttons / Indicator Lamps An operation in which a self-resetting Switch returns to its original position ...