...ndustrial Automation forward voltage Definition The appropriate product category Push Buttons / Indicator Lamps The voltage at the ends of the LED....
...trial Automation enabling hold force Definition The appropriate product category Push Buttons / Indicator Lamps The force required for the held state....
...ustrial Automation incandescent lamp Definition The appropriate product category Push Buttons / Indicator Lamps A method to provide illumination with an incandescent lamp....
...N Industrial Automation LED lighting Definition The appropriate product category Push Buttons / Indicator Lamps A method in which an LED premounted to the PCB built into the Operation Unit is...
...al Automation absolute maximum value Definition The appropriate product category Push Buttons / Indicator Lamps The value that should never be exceeded even momentarily....
...OMRON Industrial Automation LED lamp Definition The appropriate product category Push Buttons / Indicator Lamps A method in which only the light source of an incandescent lamp model is change...
...ty Components UL Certification Model Ratings Standard No. Class No. File No. D4BL Model without Indicator: A300 (Carry current: 10A) Model with Indicator: 6A, 115V AC CSA C22.2 No.0,...