...ting the machine configuration and entering the target set time. Applicable Models: Servo: G5/G/W Series, SMARTSTEP 2/SMARTSTEP Junior/SMARTSTEP A Series * Inverter: MX2/MX2-V1/RX/RX-V1/JX/MX...
...alog monitor output? Answer Yes, there is a cable available. The Analog Monitor Cable for the W-series (R88D-W) Servo Drivers can be used. The Cable's model number is R88A-CMW001S....
...control is possible by installing a DeviceNet Communications Unit (R88A-NCW152-DRT) in an OMNUC W-series Servo Driver. A DeviceNet Communications Unit provides a DeviceNet communications inte...
...turned ON. This is more clearly checked if the dummy load is a lamp with an output of about 100 W. (However, the capacity of the lamp must be within the rated range of the SSR.) MY Best-selli...
...ds can be directly switched without bleeder resistance. Bleeder Resistance 100 VAC 5 to 10 kΩ 3 W 200 VAC 5 to 10 kΩ 15 W Solid-state Relays with DC Output: Leakage current may cause...
...tor must be checked to match the load, but previous experience shows that a resistor of 100 Ω/1 W and a capacitor of 0.1 μF/250 VAC will prevent reset failure. Also, as mentioned above, the l...
...heat radiated by Solid-state Relays can be found using the following equation. Heating value P (W) = Output-ON voltage drop (V) x Carry current (A) For example, if a load current of 8 A flows...
...with the power supply to keep the Solid-state Relay ON. Bleeder Resistance 100 VAC 5 to 10 kΩ 3 W 200 VAC 5 to 10 kΩ 15 W MY Best-selling, general-purpose relays that can be selected...
...g method Surface mounting 8-pin socket 8-pin socket Flush mounting panel cutout 43.5 x 50.5 mm (W x H) (H3A-Y) 45 x 55 mm (W x H) (H3A + Y92F-40) 45 x 45 mm (W x H) (H3CR-A8...
... type Flush mounting: 1 type Mounting method Surface mounting Three M4 screw holes 74 x 102 mm (W x H) Triangle (H2E, -P, 2) 80 x 120 mm (W x H) Triangle (H2E-M, MP) Two M3 screw hol...