FAQ02116 for Solid-state Relays | OMRON Industrial...- ...will turn ON when the voltage is applied, thus maintaining the switching operation of the load. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02116/
faq02119- ... leakage current increases proportionally with the load voltage. Refer to the following graphs. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02119/
faq02128- ...as well as the fact that semi-conductors are susceptible to breakdown caused by short-circuits. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02128/
FAQ02150 for Solid-state Relays | OMRON Industrial...- ...tion while current flowing causes the SSR to burn out. Perform the proper wiring and soldering. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02150/
FAQ02152 for Solid-state Relays | OMRON Industrial...- ... G3CN-D, G3FD, or G3HD. Bleeder Resistance 5 VDC 1.6 kΩ 1/4 W 12 VDC 620 Ω 1 W 24 VDC 330 Ω 5 W MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02152/
FAQ02153 for Solid-state Relays | OMRON Industrial...- ... A max. Over 40 A 3.7 kW max. Over 3.7 kW Triac OK OK OK Not as good Two thyristors OK OK OK OK MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02153/
FAQ02155 for Solid-state Relays | OMRON Industrial...- ...e, the leakage current will increase, so check that the reset failure in item 1 does not occur. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02155/
FAQ02159 for Solid-state Relays | OMRON Industrial...- ... to the difference between the SSRs in operating time and reset time when the load is switched. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02159/
FAQ02202 for Solid-state Relays | OMRON Industrial...- ...ns with small signal currents. G3VM Solid-state Relay is available from OMRON with NC contacts. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02202/
faq02211- ...to the LOAD or to the INPUT terminal? Answer The load must be connected to the LOAD terminal. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/18/faq02211/