faq02678- ...y and directionality than E39-R1, so more light returns to the receiver, which enables a longer sensing distance. For reference, the sensing distance for E3Z-R Photoelectric Sensors ...
https://www.ia.omron.com/support/faq/answer/43/faq02678/
faq02949- ...swer No, they cannot. If they are used at the same time, the Slit will become tilted, and the sensing distance will be extremely short. Do not use them at the same time. E2E Standard Sensor...
https://www.ia.omron.com/support/faq/answer/43/faq02949/
faq03125- ...c Sensors to decrease the lens diameter and narrow the light beam. This is done to increase the sensing performance for the smallest detectable object. Usage One set of two Slits for the emit...
https://www.ia.omron.com/support/faq/answer/43/faq03125/
faq03147- ...lective surface. The anti-fog effect of the coating is similar to that used by ski goggles. The sensing distance with E39-R1K is the same as with E39-R1. For example, with E3Z-R Photoelectric...
https://www.ia.omron.com/support/faq/answer/43/faq03147/
faq03192- ... it be corrected? Answer Retroreflective Sensors normally have the MSR function, and so shiny sensing objects can also be detected. Perform a test before using Sensors for sensing ...
https://www.ia.omron.com/support/faq/answer/43/faq03192/
faq03418- ...SUS spiral coating) Overview of Model Variations Type Ambient temperature range Features Shape, sensing distance (mm)* Model number Through-beam -40°C to 150°C M4 screw 760 E32-T51 -40°C to 2...
https://www.ia.omron.com/support/faq/answer/43/faq03418/
faq00849- ..., it can. It is possible to detect more than one liquid leakage with a single K7L by connecting sensing bands in parallel with use of terminal blocks However, be aware that the ...
https://www.ia.omron.com/support/faq/answer/48/faq00849/
FAQ01249 for Ultrasonic Sensors | OMRON Industrial...- ...nfiguration of objects detected by the Ultrasonic Sensors? Answer Types and configurations of sensing objects(Reflective Type) Types and configurations of sensing objects are divid...
https://www.ia.omron.com/support/faq/answer/50/faq01249/
FAQ01275 for Ultrasonic Sensors | OMRON Industrial...- ...to the surface of Ultrasonic Sensors, is the operation affected? Answer Yes, it is. Since the sensing distance becomes shorter than the rated sensing distance, the operation in thi...
https://www.ia.omron.com/support/faq/answer/50/faq01275/
FAQ01295 for Ultrasonic Sensors | OMRON Industrial...- ...1295 Related Contents Primary Contents Question When a cover is placed on the Ultrasonic Sensor sensing surface, does it affect the sensing? Answer If the cover is within the propa...
https://www.ia.omron.com/support/faq/answer/50/faq01295/