faq02819- ...swer Yes, the Relays may become detached if the equipments are exposed to vibration or shock. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02819/
faq02820- ...ms such as deterioration and breakdown of the transistor caused by counter electromotive force. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02820/
faq02821- ... within 20 ms. 3.Diode characteristics: Withstand inverse voltage: 1,000 V Forward current: 1 A MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02821/
FAQ02822 for General Purpose Relays | OMRON Indust...- ...input pulse (input with inverse polarity of set input) puts the Relay into the reset condition. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02822/
faq02825- ...ts are suitable for operating microloads. MY4Z has a shorter electrical life. Contact Mechanism MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02825/
faq02826- .... FAQ02826 Related Contents Primary Contents Question Which Sockets and Hold-down Clips are for MY General-purpose Relays? Answer Refer to the following table. Connecting Sockets/Hold-down ...
https://www.ia.omron.com/support/faq/answer/36/faq02826/
faq02827- ...th gold-plated contacts? Answer Yes, Relays from MY4ZN-CBG General-purpose Relays, G2A, MY4Z, MY[]Q, and MY4N Series have gold-plated contacts. Even if Relays are not used and just stored, ...
https://www.ia.omron.com/support/faq/answer/36/faq02827/
faq02828- ...e parentheses. At 12 VDC R = 15 KΩ max. P = 450 mW min. At 24 VDC R = 30 KΩ max. P = 0.1 W min. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
https://www.ia.omron.com/support/faq/answer/36/faq02828/
faq02829- ...10% of the coil rating. In this case, it is 121 VAC (110 VAC x 110% = 121 V). Applicable model: MY Series MY Best-selling, general-purpose relays that can be selected based on operat...
https://www.ia.omron.com/support/faq/answer/36/faq02829/
faq02830- ...s Primary Contents Question Do you have any Relays that can switch more than 3 A? Answer Yes, MY General-purpose Relays, LY, and MK Series. MY Best-selling, general-purpose relays ...
https://www.ia.omron.com/support/faq/answer/36/faq02830/