...ppropriate product category Level Switches Unit of electrical conductance for liquids (Siemens: S). It is commonly expressed in micro-siemens (μS). It is the inverse value of electrical resis...
...In this connection, communications becomes more efficient because it is independent from master's communication cycle, but can is changeable due to data variation and requests from applicatio...
...when a set period of time elapses. Communications in this connection is independent from master's communication cycle. Cyclic connection cannot be used concurretly with COS connection....
...pectancy Definition The appropriate product category Power Supplies Typically, the Power Supply's service life depends on the service life of the aluminum electrolytic capacitors used in the ...
... for the serial communications developed by Modicon Inc.(AEG Schneider Automation International S.A.S.). The protocol is widely used in the FA and PA markets for devices such as inv...
...e Datalink Component of the CX-Integrator. It is saved in the CPU Bus Unit Area in the CPU Unit’s Parameter Area. You must keep in mind that it is not saved in the Controller Link Units....
...omotors / Servo Drivers A function that prevents the Servomotor from rotating beyond the device's travel range by connecting limit inputs. When the Forward Drive Prohibit Input or Reverse Dri...
...onitor Definition The appropriate product category Networks The total ON time of the Slave Unit's internal circuit power supply is stored. A value can also be set in the Slave Unit to enable ...
...t an load short-circuit has occurred and the output is turned OFF to prevent damage to the Unit's output circuit. The status can be checked by using the LED indicators on the Slave Unit or by...