...Automation alternate Definition The appropriate product category Push Buttons / Indicator Lamps A repeated operation in which pressing a switch once turns it ON (or OFF) and pressing...
...priate product category Programmable Controllers The basic FA Network for OMRON PLC. Connecting a Controller Link Unit to the network enables data links between PLCs so that data can be share...
...ation Controller Link Unit Definition The appropriate product category Programmable Controllers A Special I/O Unit that can be a node on a Controller Link Network, the basi...
... Units that are actually mounted are called the real I/O tables. The I/O tables registered from a Programming Device are called the registered I/O tables....
...al Automation IOM Hold Bit Definition The appropriate product category Programmable Controllers A bit in the Auxiliary Area that controls whether the status of the I/O memory is preserved whe...
...ial Automation Inner Board Definition The appropriate product category Programmable Controllers A Board that can be mounted in the CPU Unit. The CS1 and CQM1H support Inner Boards....
...or the serial communications developed by Modicon Inc.(AEG Schneider Automation International S.A.S.). The protocol is widely used in the FA and PA markets for devices such as inverters and ...
...al Automation SFC language Definition The appropriate product category Programmable Controllers A graphical programming language developed to facilitate programming step control to control se...
...SYSMAC BUS remote I/O can be used to connect Basic I/O Units or Special I/O Units by connecting a Slave Rack. It can also be used to connect Remote Terminals or Relay Terminals....