...omation alarm/event function Definition The appropriate product category Programmable Terminals A function that reports alarms based on changes in bit status. There are two functional objects...
...ess Definition The appropriate product category Programmable Controllers The network address of a Network Communications Unit that is mounted alone on the CPU Unit with no local network table...
...trial Automation Host Link Definition The appropriate product category Programmable Controllers A serial communications mode allowing the I/O memory of the CPU Unit to be read and written, an...
...al Automation symbol table Definition The appropriate product category Programmable Controllers A table that defines global symbols and local symbols in the CX-Programmer....
...tion CT input Definition The appropriate product category Temperature Controllers An input from a current transformer (CT) is used to measure the current flowing to the heater. The input sign...
...l Automation bank function Definition The appropriate product category Digital Panel Indicators A function that allows up to eight sets of comparison settings as well as prescaling values to ...
... Definition The appropriate product category Photoelectric Sensors The angle where operation as a Photoelectric Sensor is possible for a Through-beam Sensor or Retro-reflective Senso...
...tion mode Definition The appropriate product category Photoelectric Sensors One of the modes of a Fiber Amplifier Unit, this mode provides more-precise detection and a longer sensing...
...peed mode Definition The appropriate product category Photoelectric Sensors One of the modes of a Fiber Amplifier Unit, this mode provides faster response time than the standard mode. The sen...
...ier Definition The appropriate product category Photoelectric Sensors Through-beam Sensors have a separate Emitter and Receiver while Reflective Sensors have an integrated Emitter and Receive...