| Site Search | Product Search | IA Global Search |
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
...le and can be adapted to perform a wide variety of tasks and applications. We’re also scalable, so we can grow with your business. Grow Your Business − Modify layouts to optimize production A...
...herCAT or EtherNet/IP network communications. Other Units are available for expansion racks and so on....
https://www.ia.omron.com/products/category/automation-systems/programmable-controllers/cj2/
...utomated machinery with a pudding production line. Counters are often mounted on control panels so that the workers can check the display. Pudding Production Line The operation of a Preset Co...
...ut Capacity Output capacity (W) = Output voltage (V) × Load current (I) Select the Power Supply so that the maximum load capacity will be lower than the rated output capacity. Note:The output...
...ntroller NX Series Catalog F104-E1-03 Correction Notice NX-series Safety Control Units NX-SL/SI/SO Datasheet CSM_NX-SL_SI_SO_E_4_6 Correction Notice Catalog English Corrected catalog...
..., or hexadecimal codes. Visually checking initial values The selected value is displayed as is, so you can always check the set value visually. This makes it easier to prevent incorrect opera...
...ifications and Structures What Is a Pushbutton Switch? A Pushbutton Switch is a switch designed so that its contacts are opened and closed by depressing and releasing a pushbutton on the Swit...
...cam control. Concerning Motion Controllers, OMRON offers different products in different areas. So please click on the banner "Products links" in the top right corner to reach the country web...
...explosion-proof areas. However, the lens, the case, and the fiber covering are made of plastic, so they must be free from corrosion or deterioration (fogging) due to contact with solvents. As...
...e lead wires and the power line for the Temperature Sensor are routed through the same conduit, so the lead wires are affected by noise from the power line. (Ordinarily, this causes the displ...
...use it’s easier to aim at the desired terminal. Safety The structure provides finger protection so that your fingers never touch conductive parts. Minimum Width of 3.5 mm to Help Downsize Con...
...No special safety measures required for Class 1 laser The E3AS Series is classified as Class 1, so laser safety measures are not required. *1. The reference values were measured using the OMR...
...ngle characteristics of ±85° max. Place the sensors away from the pathways of people and robots so that the sensors do not obstruct their movement. Thus remove failure risks such as optical a...
... high-frequency switching. Unlimited number of switching operations. Consist of semiconductors, so there is no contact erosion caused by switching. Zero cross function. No operation noise. Et...
...will weaken. The power of the release spring will become stronger than the magnetic attraction, so the armature will release and the relay will be in the relaxed state. When the armature has ...
...ontrollers are mainly used for heater control. Each heater control method has its own features, so it is necessary to decide the method that matches your application. Heater Control Methods (...
... be replaced during power supply or operation. In addition, cable disconnections are monitored, so failures can be located easily. Remove or add units without using a programming device The d...
...system, with its highly stable light source, can be turned off when illumination is not needed. So, electricity costs can be reduced. (For a lamp system whose light source is unstable, you ha...