| Site Search | Product Search | IA Global Search |
...n Amplifier English 日本語 Print Page Image Sensing method Through-beam type Sensing distance 10 m Light source Red LED (660 nm) Connection method M8 connector models Item list of E3Z Ratings...
...n Amplifier English 日本語 Print Page Image Sensing method Through-beam type Sensing distance 30 m Light source Infrared LED (870 nm) Connection method M8 connector models Item list of E3Z Ra...
... at 48 VDC Inrush current NC: 30 A max. NO: 20 A max. Indicator LED, Possible to change between Light when operating and Light when not operating. Conduit G1/2 Ambient temperature Op...
...SX470 Photomicrosensor, Slot type, Through-beam, Standard, Sensing distance: 5 mm (slot width), Light-ON, Indicator: Incident light, NPN output, Connector model EE-SX471 Photomicrose...
... distance. Narrow View (Detection Across clearance) • The fine beam prevents false detection of light that is reflected off surrounding objects. Detection without Background Interference • Th...
... FA sites. High-precision and reliable position detection is possible without being affected by light interference and backgrounds. Search This is a standard search inspection item. This type...
...el Number Description E3JK-DN11 2M Photoelectric Sensor, DC power type, Diffuse-reflective, Red light, Sensing distance: 2.5 m, NPN output, Pre-wired, 2 m E3JK-DN12 2M Photoelectric Sensor, D...
..., the coloring also affects the power of the laser. To completely block the laser beam, a laser light curtain can be used. The specified wavelength of the V500-R521 is 650 nm. Helium-Neon (He...
...dustrial Automation Fiber Sensors Fiber Sensors List With these Separate-amplifier Sensors, the light from the Amplifier is transmitted through a fiber to enable detection in narrow places, o...
https://www.ia.omron.com/products/category/automation-systems/networks/io-link/fiber-sensors/
...M2PA-90A12-12EW Indicator (Square), Square, Single screen, White, LED (12 VAC/VDC), Case color: Light gray M2PA-90A12-24EG Indicator (Square), Square, Single screen, Green, LED (24 VAC/VDC), ...
...y Inverters A function that automatically saves excess energy that is consumed when the load is light. It works by automatically reducing the output voltage when operation is at a constant sp...
...ock function. An auto-reset does not use an interlock. For example with the Through-beam Safety Light Curtain, after the power is turned ON and the Safety Light Curtain beam is inter...
...etween the sensors and display. Works with a touch of anything. Relatively lower durability and light transmittance due to the membrane surface. Lower production cost than other methods. Resi...
https://www.ia.omron.com/support/guide/27/further_information.html
...inclination of the object. In the case of (B) and (C), stray reflectons occur and the reflected light is not uniform, however, the effect of inclination is small. PDF Download(865KB) Local Na...
https://www.ia.omron.com/support/guide/50/explanation_of_terms.html
...Contents Lead Contents Power Supplies Uninterruptible Power Supplies (UPS’s) Axial-flow Fans UV-Light Curing Systems Static Electricity Components Laser marker Inspection System Power/Compone...
.../672 (Reflective, Sensitivity Adjustor) EE-SX67/47 EE-SPX302/304/306/402/404/406-W2A (Modulated Light) EE-SPX301/401 (Modulated Light) EE-SPY311/312/411/412 (Convergent Reflective, M...
...r Power Supplies & In Addition Related Contents Lead Contents Power Supplies Axial-flow Fans UV-Light Curing Systems Static Electricity Components Laser marker Power/Component Protective Comp...
.../672 (Reflective, Sensitivity Adjustor) EE-SX67/47 EE-SPX302/304/306/402/404/406-W2A (Modulated Light) EE-SPX301/401 (Modulated Light) EE-SPY311/312/411/412 (Convergent Reflective, M...
...periodically during operation. This function is called self testing for F3SN/F3SH Series Safety Light Curtains. Applicable models: F3SL Series Safety Light Curtain F3SS-AT60P Single-...
...aller compared with an Solid-state Relay. Solid-state Relay: Leakage current causes the lamp to light dimly. A bleeder resistor is added to prevent this. The Solid-state Relay requires a snub...