| Site Search | Product Search | IA Global Search |
...f TP70 Related Contents Common Cautions Technical Guide Models with Standards Certification FAQ Limit Switches Item A to Z Index Glossary of Industrial Automation Features Lineup Specificatio...
https://www.ia.omron.com/products/family/304/download/catalog.html
... of VE Related Contents Common Cautions Technical Guide Models with Standards Certification FAQ Limit Switches Item A to Z Index Glossary of Industrial Automation Features Lineup Specificatio...
https://www.ia.omron.com/products/family/333/download/catalog.html
...ensor includes all sensors that perform non-contact detection in comparison to sensors, such as limit switches, that detect objects by physically contacting them....
... connector. A Sensor I/O Connector is connected to a Photoelectric Sensor, Proximity Sensor, or Limit Sensor that has a connector or prewired connector....
... objects. The most common types of auto-tuning are the step response, marginal sensitivity, and limit cycle methods....
... voltage Definition The appropriate product category Push Buttons / Indicator Lamps The voltage limit when a reverse voltage is applied....
...N Industrial Automation permissible operating force Definition The appropriate product category Limit Switches The maximum load that can be applied to an actuator during operation....
...ON Industrial Automation pull-out strength of cable Definition The appropriate product category Limit Switches The maximum pull that a cable and the cable connection can withstand....
... | OMRON Industrial Automation Free Position Definition The appropriate product category Safety Limit Switches The Actuator position when no external force is applied. The free position is gi...
... the comparison values. Comparison outputs 1 and 2 can be set to one of three operations: upper limit alarm, lower limit alarm, or upper/lower limit alarm....
...OMRON Industrial Automation output current capacity Definition The appropriate product category Limit Switches The allowable current of an output circuit....
...ex | OMRON Industrial Automation snap-action Definition The appropriate product category Safety Limit Switches A construction in which a moving contact can move quickly from one fixed contact...
...lossary index | OMRON Industrial Automation contact Definition The appropriate product category Limit Switches The metal parts that touch when the movable plate reverses to perform electrical...
...RON Industrial Automation Total Travel Force Definition The appropriate product category Safety Limit Switches The force that must be applied to the Actuator to move from the free position to...
...d to the operating circuits. The appropriate product category Timers The time required for time-limit contacts to complete operation for the specified input....
...tegory Temperature Controllers The upper and lower limits for the MV are set by using the upper limit and MV lower limit settings. When the MV calculated by the Temperature Controlle...
...ndustrial Automation direct opening position Definition The appropriate product category Safety Limit Switches The Actuator position where the moving contacts are directly opened when an exte...
...N Industrial Automation direct opening force Definition The appropriate product category Safety Limit Switches The force needed to be applied to the Actuator to move from the operating positi...
...dex | OMRON Industrial Automation electrical rating Definition The appropriate product category Limit Switches The basic current, voltage, and load conditions used as a standard when using a ...
...N Industrial Automation electrical durability curve Definition The appropriate product category Limit Switches A curve that gives the change in durability for specific electrical usage condit...