| Site Search | Product Search | IA Global Search |
...trial Automation operating position repeat accuracy Definition The appropriate product category Limit Switches The width of change in the operating position during repeated operation....
...| OMRON Industrial Automation operating sensitivity Definition The appropriate product category Limit Switches The electric capacity or the resistance between the antenna and ground required ...
... OMRON Industrial Automation Operating Force Definition The appropriate product category Safety Limit Switches The force needed to be applied to the Actuator to move from the free position to...
...dex | OMRON Industrial Automation Pre-Travel Definition The appropriate product category Safety Limit Switches The distance or angle through which the Actuator moves from the free position to...
...ex | OMRON Industrial Automation operating capacity Definition The appropriate product category Limit Switches The electric capacity between the Antenna and ground required to perform detecti...
...for comparison outputs. This enables outputs for changes in levels rather than just upper/lower limit comparisons to set value. It can be set according to the control applications. Note: The ...
...- Glossary index | OMRON Industrial Automation head Definition The appropriate product category Limit Switches For a Limit Switch, a part with a mechanism that functions independentl...
...rce necessary to reverse the direction of the lever Definition The appropriate product category Limit Switches The force required to move the actuator of a Fork Lever Lock Switch from the fre...
...strial Automation movement until the lever reverses Definition The appropriate product category Limit Switches The movement distance (or angle) to move the actuator of a Fork Lever Lock Switc...
... index | OMRON Industrial Automation operation part Definition The appropriate product category Limit Switches The position to operate an actuator. In case of rod actuators, the position is d...
...omation set point limiter Definition The appropriate product category Temperature Controllers A limit within which the set point range is controlled to prevent a controlled object from being ...
... - Glossary index | OMRON Industrial Automation dog Definition The appropriate product category Limit Switches An operating object provided on the moving part of a machine to press or return ...
...lossary index | OMRON Industrial Automation spatter Definition The appropriate product category Limit Switches The zinc powder produced when welding. Adhering spatter to the Limit Sw...
...ssary index | OMRON Industrial Automation separator Definition The appropriate product category Limit Switches A device used to increase separation when the insulation distance may be insuffi...
...sary index | OMRON Industrial Automation DOP Definition The appropriate product category Safety Limit Switches An acronym for direct opening position....
...sary index | OMRON Industrial Automation DOF Definition The appropriate product category Safety Limit Switches An acronym for direct opening force....
...ex | OMRON Industrial Automation clearance distance Definition The appropriate product category Limit Switches The minimum distance through space between two charged parts....
...ction that prevents the Servomotor from rotating beyond the device's travel range by connecting limit inputs. When the Forward Drive Prohibit Input or Reverse Drive Prohibit Input turns OFF, ...
...o the Unit or the calculated data for the Unit can be compared with alarm settings (upper upper limit, upper limit, lower limit, and lower lower limit) and the resu...
...dex | OMRON Industrial Automation terminal strength Definition The appropriate product category Limit Switches The tightening torque for terminal screws of switches when wire leads. In case o...