| Site Search | Product Search | IA Global Search |
...DC and Low Voltage 24 to 48 VAC/12 to 48 VDC. • ON- and OFF-times can be set independently and so combinations of long ON- or OFF-time and short OFF- or ONtime settings are possible. • Twen...
... design. It offers greater performance and faster I/O response as well as extreme scalability - so you will only need one family. In addition, programming, debugging and networking are faster...
... to maintain a stable measurement. They are also susceptible to the influences of ambient light so are difficult to measure using conventional laser measurement sensors. The ZG2 solves these ...
...nd power factors to appropriate levels. Fixed values are used for the voltage and power factor, so the accuracy specifications do not apply. * Set the voltage to 100 V when performing simple ...
...ircuit. Two Outputs: Light-ON and Dark-ON All models provide both a light-ON and dark-ON output so that the output can be switched according to the application simply by changing the wiring. ...
...d I/O signals (12/8 and 0/32). Function blocks up to 128pcs complete this fully flexible range, so you can always be sure of a needs-match solution. Simple Above all, the Omron G9SP range is ...
...even when the door closes slowly. No adhesion of iron particles Permanent magnets are not used, so iron is not attracted, making maintenance easier. Visible safety Checking at the production ...
...plastic rod actuator makes the Switch easy on hands. • One-way operation: Equipped with stopper so that operation is only possible from one direction. • Distinctive yellow used for the body. ...
... easily. It allow you to edit the program on the controller and the compiling is not necessary. So you can develop and adjust the system quickly. ・Microsoft® Visual Studio® and Windows are ei...
...reviously they could not go. Moreover, you can select a size according to the area of coverage, so targets are uniformly neutralized. Easy installation Ideal for narrow workbenches to wide li...
...ght Interference Operation is possible with ambient illumination of up to 80,000 lx (sunlight), so the Code Reader can stably read even near Photoelectric Sensors with little influence from a...
...ew or installation distance that is best for the equipment type. Both models are the same size, so additional design work is not necessary to change the model. Reading Test Switch Provided We...
...ate: May 30, 2013 Mount Using M2 or M3 Screws The EE-SX95 can be mounted using M2 or M3 screws, so it can easily replace an existing Sensor mounted with M2 screws. Reliable Best-in-Class Sens...
...strial environments. These people also wanted attractive pricing, without compromising quality. So we put to work our 50-year heritage in proximity sensors: a heritage that has seen 200 milli...
...P60) Mist Molded terminal 139 type (WL[]-139-N/WL[]-139) The SC connector can be removed, so it is possible to use flexible conduit for the cable. (WL[]-RP40-N/WL-RP40) Constant wate...
...e the optical fiber, preventing stable detection. Easy Cable Routing The cable opening is wide, so the cable can be routed easily. Hex shape Provides Simplicity and Reliability Full lineup of...
...along with the program progression (PRG and SEG (yellow)). These are all visible simultaneously so that you don’t have to switch the display. *2. Excluding the E5CC-T. The program and segment...
...along with the program progression (PRG and SEG (yellow)). These are all visible simultaneously so that you don’t have to switch the display. *2. Excluding the E5CC-T. The program and segment...
...along with the program progression (PRG and SEG (yellow)). These are all visible simultaneously so that you don’t have to switch the display. *2. Excluding the E5CC-T. The program and segment...
...rther “Ease of Use” Contact Status at a Glance Mechanical indicators are now a standard feature so that you know the contact operating status even for standard models. No Need for Coil Energi...