Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 3801 - 3820 of 43944
Control Components - Product Category | OMRON Indu...

...input values to set values, transfer data, and perform other functions. Voltage / Current Input Load Cell Input Pulse Input Temperature Input Voltage / Current / Pulse Input Signal converters...

https://www.omron-ap.co.in/products/category/control-components/

S8V-CP DC Electronic Circuit Protector (24 VDC 4 O...

...vices Shortening Lead Time for Control Panel Building Easier setting and wiring reduce the work load of operators Sequential start-up of branch circuits can avoid the trouble of operation sta...

https://www.omron.com.tw/products/family/3780/

trigger circuit - Glossary index | OMRON Industria...

...ct category Solid-state Relays A circuit that controls a trigger signal for a triac switching a load current....

https://www.ia.omron.com/support/glossary/meaning/103.html

bleeder resistance - Glossary index | OMRON Indust...

...The appropriate product category Solid-state Relays The resistance connected in parallel to the load to increase an apparently small load current, so that the ON/OFF of minute curren...

https://www.ia.omron.com/support/glossary/meaning/124.html

TV rating (UL/CSA) - Glossary index | OMRON Indust...

...he UL and CSA standards. It is one of the typical ratings. The TV rating indicates the level of load that can be switched by the Relay, including the inrush current....

https://www.ia.omron.com/support/glossary/meaning/13.html

Servomotors - Glossary index | OMRON Industrial Au...

... servo system and is used with a Servo Drive. The Servomotor includes the motor that drives the load and a position detection component, such as an encoder....

https://www.ia.omron.com/support/glossary/meaning/160.html

starting torque - Glossary index | OMRON Industria...

...egory Inverters The torque that is output when the motor starts. The motor will not rotate if a load larger than this torque is applied to the motor....

https://www.ia.omron.com/support/glossary/meaning/2943.html

permissible operating force - Glossary index | OMR...

...missible operating force Definition The appropriate product category Limit Switches The maximum load that can be applied to an actuator during operation....

https://www.ia.omron.com/support/glossary/meaning/2956.html

maximum switching capacity - Glossary index | OMRO...

...itching capacity Definition The appropriate product category General Purpose Relays The maximum load capacity that can be switched. Design circuits to ensure that this value is not exceeded d...

https://www.ia.omron.com/support/glossary/meaning/30.html

residual voltage - Glossary index | OMRON Industri...

...een the output line (the black wire) and the 0-V line (the blue wire). A relay, timer, or other load is connected between the power supply line (the brown wire) and the output line (the black...

https://www.ia.omron.com/support/glossary/meaning/3033.html

vibration class - Glossary index | OMRON Industria...

...e value of the vibration measured at the shaft of a motor rotating at the rated speed without a load. There are five vibration classes into which the measured total amplitudes are divided....

https://www.ia.omron.com/support/glossary/meaning/3091.html

strain gauge - Glossary index | OMRON Industrial A...

... electric resistance of the strain gauge changes when the gauge is elastically deformed under a load. If a constant voltage is applied, the size of the current flowing can be used to measure ...

https://www.ia.omron.com/support/glossary/meaning/3108.html

contact capacity of output - Glossary index | OMRO...

...ntact capacity of output Definition The appropriate product category Level Switches The maximum load that can be switched by the 61F Level Controller....

https://www.ia.omron.com/support/glossary/meaning/3144.html

derating curve - Glossary index | OMRON Industrial...

...cifies the operating conditions that are required at various ambient operating temperatures and load rates to ensure that Power Supply specifications are met....

https://www.ia.omron.com/support/glossary/meaning/3234.html

electrical rating - Glossary index | OMRON Industr...

...ting Definition The appropriate product category Limit Switches The basic current, voltage, and load conditions used as a standard when using a Switch....

https://www.ia.omron.com/support/glossary/meaning/3247.html

electrical durability curve - Glossary index | OMR...

...ves the change in durability for specific electrical usage conditions such as current, voltage, load, etc. in graph format. The durability depends on test conditions, so the data is for refer...

https://www.ia.omron.com/support/glossary/meaning/3250.html

remote sensing function - Glossary index | OMRON I...

...duct category Power Supplies Remote sensing can be used to compensate for a voltage drop on the load lines. (The compensation range is ±10% of the rated output voltage.)...

https://www.ia.omron.com/support/glossary/meaning/3467.html

proportional action - Glossary index | OMRON Indus...

...he deviation between the process value and the set value. The normal set value is at 50% of the load rate. With only proportional control, the process value and set value will not be balanced...

https://www.ia.omron.com/support/glossary/meaning/3620.html

contact relay output - Glossary index | OMRON Indu...

...emperature Controller is generally small and not sufficient for driving a heater or other large load. The output is thus used with an external electromagnetic contactor....

https://www.ia.omron.com/support/glossary/meaning/3648.html

phase angle control - Glossary index | OMRON Indus...

...ategory Temperature Controllers A method for controlling the time that power is supplied to the load. Phase angle control enables changing the phase angle of an AC voltage applied to a ...

https://www.ia.omron.com/support/glossary/meaning/3681.html

Results 3801 - 3820 of 43944

Select Country in