| Site Search | Product Search | IA Global Search |
...xpected service life calculation assumes the following conditions: (1) Rated input voltage, (2) Load rate: 50%, (3) Ambient operating temperature: 40C, (4) Standard mounting position, (5) Con...
...sic Switches A switch with a plunger that has a larger plunger diameter than a pin plunger. The load must be aligned with the center of the plunger to prevent eccentricity when the switch is ...
...dustrial Automation regenerative energy Definition The appropriate product category Inverters A load connected to a motor has kinetic energy while it rotates and has potential energy while it...
...od used when autotuning cannot be performed due to the restrictions of the operating pattern or load conditions or when maximum responsiveness needs to be obtained for individual loads....
...hing capacity Definition The appropriate product category Proximity Sensors The maximum size of load that can be switched by the output of a proximity sensor....
...on The appropriate product category Timers The life when a control output is operated without a load....
...ition The appropriate product category Timers The life when switching the control output with a load of the specified voltage and current applied....
...egory Inverters The torque that is output when the motor starts. The motor will not rotate if a load larger than this torque is applied to the motor....
...ts). The data being measured is either analog data, such as a temperature, current, voltage, or load cell signal, or digital data, such as a pulse signal....
...inst external noise.The noise resistance of the Timer is checked with a noise simulator, a coil load, an oscillating relay, and static electric noise....
...to the AC input terminals. This value is the stable current and will fluctuate depending on the load....
...tion The appropriate product category General Purpose Relays The durability of contacts when no load is applied and the contacts are switched at a specified switching frequency. The appropria...
...Definition The appropriate product category Signal Converters When AC voltage E is applied to a load (e.g., a device), the phase of the AC current I flowing in it generally lags behind or lea...
...ion The appropriate product category Temperature Controllers A circuit that is connected to the load through the collector of the transistor, which is extended externally. The appropriate pro...
...ategory Solid-state Relays The current that can flow into the output terminals when a specified load voltage is applied to the SSR with the output turned OFF....
...mechanical conditions under which the customer uses the device, including the current, voltage, load type, operating frequency, and operating speed....
...The appropriate product category Solid-state Relays A circuit that starts operation with the AC load voltage at close to zero-phase....
...ate product category Solid-state Relays A function that suppresses noise for rapid increases in load current by turning ON the Relay near the zero voltage of the AC load power supply...
...elay can withstand when the voltage surges momentarily due to lightning, switching an inductive load, etc. The surge waveform, unless otherwise specified, is the standard impulse voltage wave...
...e appropriate product category General Purpose Relays The durability of contacts when the rated load is applied and the contacts are switched at a specified switching frequency. The appropria...