Primary Contents

IA Global Search Results

Select Country in

Site Search Product Search IA Global Search
Results 5661 - 5680 of 42303
faq00752

...ntents Primary Contents Question I'm using General-purpose 61F Floatless Level Controllers with cable conductor of 2 mm2 and a length that is less than 1 km, but it malfunctions. Is there a s...

https://www.ia.omron.com/support/faq/answer/33/faq00752/

faq00755

...wo lock nuts. If the Electrodes are too long, it may cause problems with strength and handling. Cable-type Electrodes (PH) or Electrode Bands are more suitable. Application Model Features and...

https://www.ia.omron.com/support/faq/answer/33/faq00755/

FAQ00844 for Level Switches | OMRON Industrial Aut...

...s Primary Contents Question Is it acceptable to wire 61F's Floatless Level Controller electrode cable and power cable in the same duct? Answer  There is a possibility of improper op...

https://www.ia.omron.com/support/faq/answer/33/faq00844/

FAQ00955 for Rotary Encoders | OMRON Industrial Au...

...e output current and thus the rising and falling speeds of signals are fast. This allows a long cable distance. They can be connected to open-collector input devices (NPN, PNP). E6C3-CWZ5GH E...

https://www.ia.omron.com/support/faq/answer/34/faq00955/

FAQ00969 for Rotary Encoders | OMRON Industrial Au...

...ead Contents FAQ No. FAQ00969 Related Contents Primary Contents Question How many meters of the cable of the Rotary Encoder are extended? Answer  Voltage output and open collector output typ...

https://www.ia.omron.com/support/faq/answer/34/faq00969/

FAQ00978 for Rotary Encoders | OMRON Industrial Au...

... is almost possible by making cut face "D" of the shaft and the direction of drawing out of the cable as the following figure. (within ±15°) E6C3-CWZ[][]H 3. Please confirm ON point of phase ...

https://www.ia.omron.com/support/faq/answer/34/faq00978/

FAQ01004 for Rotary Encoders | OMRON Industrial Au...

...e change of output data and reading timing by becoming long at the rise time of signal when the cable is extended. We recommend the rotary encoder with the strobe signal that informs of readi...

https://www.ia.omron.com/support/faq/answer/34/faq01004/

FAQ02207 for General Purpose Relays | OMRON Indust...

....01 to 0.12 8 8 0.12 to 0.14 7 9 0.14 to 0.15 6 10 0.15 to 0.18 5 12 0.18 min. 4 15 Note: 1.CVV cable: Nominal conductor cross-section area: 2 mm 2 (7 conductors), Floating capacity between w...

https://www.ia.omron.com/support/faq/answer/36/faq02207/

faq02761

...y from a distance? Answer  The distance depends on the type and installation conditions of the cable. Wiring power supplies over a long distance in parallel with power lines may cause reset ...

https://www.ia.omron.com/support/faq/answer/36/faq02761/

faq02770

...al-purpose Relays? Answer  The distance depends on the type and installation conditions of the cable. Both ends of the Relays coil must measure at least 90% of the rated coil voltage to oper...

https://www.ia.omron.com/support/faq/answer/36/faq02770/

faq02799

....01 to 0.12 8 8 0.12 to 0.14 7 9 0.14 to 0.15 6 10 0.15 to 0.18 5 12 0.18 min. 4 15 Note: 1.CVV cable: Nominal conductor cross-section: 2 mm 2 (7 conductors), Float capacitance between wires:...

https://www.ia.omron.com/support/faq/answer/36/faq02799/

faq02828

... wires or leakage current when Relays is OFF. This may also cause reset failure. Check with the cable manufacturer for how much float capacitance the cables retain. Also check the amount of l...

https://www.ia.omron.com/support/faq/answer/36/faq02828/

faq00380

...graded because of degradation of the internal filling resin, sensing surface resin material, or cable sheath due to ultraviolet light. Stress on Filling Resin Due to Sudden Temperature Change...

https://www.ia.omron.com/support/faq/answer/41/faq00380/

FAQ00402 for Proximity Sensors | OMRON Industrial ...

...ntents FAQ No. FAQ00402 Related Contents Primary Contents Question Is it possible to extend the cable of the Proximity Sensor? Answer  Yes, it provides as follows in each type of the sensor....

https://www.ia.omron.com/support/faq/answer/41/faq00402/

faq00414

...e not subjected to high temperatures. Heat-resistant parts are used for the case, solder, coil, cable and other components of the head section used in high temperatures. These Sensors, howeve...

https://www.ia.omron.com/support/faq/answer/41/faq00414/

faq02669

... above is the same for coaxial and shielded robot cables. Reference Information: For a standard cable, a minimum bending radius of three times cables diameter is recommended. E2E Standard Sen...

https://www.ia.omron.com/support/faq/answer/43/faq02669/

FAQ03429 for Vision Sensors | OMRON Industrial Aut...

...ow can a stored image that is displayed on F160 Vision Sensor be re-measured? Is there a Camera Cable for F150-VS Vision Sensor that can withstand bending? Can the camera cable for t...

https://www.ia.omron.com/support/faq/answer/44/faq03429/

FAQ03432 for Vision Sensors | OMRON Industrial Aut...

... Primary Contents Question Console cables for Vision Sensors can be extended? Answer  Standard cable length of the Console "F150-KP" is 2m. Other than this, however, cables of 5m and 10m len...

https://www.ia.omron.com/support/faq/answer/44/faq03432/

faq00849

...hen wiring, be sure not to exceed the maximum possible wiring distances for both the connecting cable and the Sensing Band. Exceeding these distances may lead to faulty operation. Connect one...

https://www.ia.omron.com/support/faq/answer/48/faq00849/

FAQ01281 for Ultrasonic Sensors | OMRON Industrial...

...sors Lead Contents FAQ No. FAQ01281 Related Contents Primary Contents Question How long can the cable for an Ultrasonic Displacement Sensor or Ultrasonic Sensor be extended? Answer  1. E4PA ...

https://www.ia.omron.com/support/faq/answer/50/faq01281/

Results 5661 - 5680 of 42303

Select Country in