| Site Search | Product Search | IA Global Search |
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...perating mode Incremental type Mounting method Flush mounting Direct mounting on PC board Count input No-voltage input DC voltage input Multi-voltage No-voltage ...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
... FAQ03357 Related Contents Primary Contents Question When inputs CP1 and CP2 are simultaneously input to H7CX Multifunction Preset Counters when used as a dual counter, are both of them count...
...that 60 (seconds) ÷ 30 (revolutions) = 2 (seconds per revolution) Therefore a pulse is normally input every 2 seconds. When the rate of rotation falls to 10 revolutions per minute (10 rpm), 6...
...Current Signals E5CN-H A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function. H5CZ Easy to Use and Easy...
...in the main circuit. An error is detected when a low voltage was detected in the main circuit's input section and lasted longer than 50 ms. The likely causes of the error are that the main vo...
...ve the rubber cap and check that the set bolt is loose. 2. Insert the Servomotor shaft into the input shaft. 3. Tighten the Servomotor installation bolt according to the tightening torque spe...
...ys Lead Contents FAQ No. FAQ02279 Related Contents Primary Contents Question What is an inverse input? Answer An inverse input is an input that creates a potential differe...
...en there is no reset switch in the feedback circuit and the device automatically starts when an input turns ON. A manual reset is when there is a reset switch in the feedback circuit and the ...
... Contents FAQ No. FAQ02416 Related Contents Primary Contents Question What is a positive common input? Answer It is an input mode where there are two inputs and both of them are co...
...nt. Solid-state Relays with a zero cross function using a photocoupler can operate with a small input current because they have very good coupler transmission efficiency. Photocoupler ...
...state Relays Lead Contents FAQ No. FAQ02044 Related Contents Primary Contents Question Does the input current change for Solid-state Relays with a wide rated input voltage? Answer ...
...ng Method Connect a load and power supply, and check the voltage of the load terminals with the input ON and OFF. The output voltage will be close to the load power supply voltage with the SS...
... those of the G2R-1A-S and so these models can be easily exchanged. Note:Be sure to confirm the input voltage, polarity, and output capacity. 3.Applications with high-voltage DC loads. To swi...
...tate Relay load Relays sometimes hum? Answer Leakage current flows when the Solid-state Relay input is OFF. If a small Relay is driven, this Leakage current may cause the Relay coil to beco...
...r AC load switching use thyristors and triacs as output elements. By turning Solid-state Relays input ON, the output can be turned ON, but simply turning the input OFF doesn't mean t...
...oltage generated. 2. Malfunction caused by external surge An external surge may suddenly damage input or output elements. A load short circuit may also cause malfunction. Design a safety circ...
...at is causing this and what can be done about it? Answer There may be separate causes for the input side and the output side. The following provides separate explanations. Input Si...
...1 Related Contents Primary Contents Question Should the load be connected to the LOAD or to the INPUT terminal? Answer The load must be connected to the LOAD terminal. MY Best-selling, gene...