| Site Search | Product Search | IA Global Search |
...fore the ending month and day. The calendar timer bit is ON between April 1 and August 31. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...w. (Fig. A) Example of an Incorrect Loopback Program (Fig. B) Example of a Correct Program K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...the menu. With "-V2" CPU Units, "V03.00" will be displayed as the system software version. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... Outputs Allows only timer number and trigger/reset settings. The Support Software Example K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ontact turns OFF? (downward differentiation) Answer See the program example given below. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...it possible to connect an NPN sensor? Answer Yes, you can.(Except the pre-V1 CPU units.) K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...cuit for Normal Operation Example 1. Example 2. Passing Input Status through Work Bits (M) K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...ing/clearing password Changing backlight OFF time Setting input filter Setting node number K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...dar timers can be changed through front-panel buttons without touching the ladder program. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...e contact turns ON? (upward differentiation) Answer See the program example given below. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...tch) has priority if I0 (forward switch) and I1 (reverse switch) turn ON at the same time. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...g on the program structure, the number of Expansion Units connected, and RS-485 interface. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...eekly timer turns ON for 15 minutes 30 seconds from 8:15 every day from Tuesday to Friday. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...EEPROM) inside the ZEN? Answer No, because the program is saved automatically to EEPROM. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
.../O Unit on the left. Inputs are allocated through Xb and outputs are allocated through Yb. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...he user's ladder program and parameter settings are stored in Flash Memory inside the ZEN. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
... Question ZEN Programmable Relays: Can I revise the program during operation? Answer No. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...the day settings are set, they do not have to reset again. It even adjusts for leap years. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...e can be set in seconds, minutes, and hours in a setting range from 0.01 s to 99 h 59 min. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...
...llows you to authorize/prohibit setting changes and parameter monitoring during operation. K3HB-X A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current ...