Page top

Lead Contents

FAQ04298 of Programmable Relays FAQ

FAQ No. FAQ04298

Primary Contents

Question

ZEN Programmable Relays: Why can't I set the parameters for the timer, counter, etc?

Answer



The timers, counters and other parameters are set with inputs in the ZEN and the Support Software. They cannot be set with outputs.

FAQ04298_Fig1

Timer Parameter Setting Window for Inputs

Allows timer type, set value, and other settings.

FAQ04298_Fig2

The Support Software Example

Timer Parameter Setting Window for Outputs

Allows only timer number and trigger/reset settings.

FAQ04298_Fig3

The Support Software Example

Recommended Products

K3HB-X

A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals

E5CN-H

A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.

H5CZ

Easy to Use and Easy to Read.

Other Programmable Relays FAQ