| Site Search | Product Search | IA Global Search |
...rating time is given for a coil temperature of 23°C or higher. The bounce time is not included. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...arry current 10 A Maximum switching voltage 250 VAC 125 VDC Maximum switching current 10 A 10 A MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...t contact with foreign material by means of enclosure in a case (designed for manual soldering) MY Some protection (No large dust or dirt particles inside Relay.) No protection Plastic sealed...
...to touch the current-carrying parts. These Sockets have an "-E" at the end of the model number. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...2760 Related Contents Primary Contents Question The terminal arrangement printed on the case of MY General-purpose Relays appears to be reverse compared to the terminal numbers indicated on t...
... MY4 with CW Cable Answer: Value exceeds 3,000 m so there is no problem with cables up to 3 km. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...000 operations as the minimum test condition, whereas MY2 specifies 500,000 operations minimum. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...n order to switch a 0.5-A DC inductive load? Answer: Keep the voltage below 50 VDC (blue line). MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...elded contacts, OFF faults, abnormal consumption, and increase of contact resistance may occur. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ccurs between them), thus all loads are instantaneously applied to only a single contact point. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...pply phase at which power is interrupted, but generally the contacts may open after about 1 ms. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...the NO contacts turn OFF. For double-pole contacts, it is the time until the NC contacts close. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...DC Maximum switching current 5 A Contact form DPDT Contact structure Single Contact material Ag MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...: For MY4 Relays 24 VDC MY4 with CVV Cable Answer: The cable needs to be within approx. 4.2 km. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...h load) the counter electromotive force is generated. Allow for a margin when selecting Relays. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... built-in diode will short-circuit, damaging not only Relays, but possibly also power supplies. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...Lead Contents FAQ No. FAQ02773 Related Contents Primary Contents Question What does the “D2” in MY[]N-D2 General-purpose Relays indicate? Answer It indicates that the relays have a built-in...
...pply phase at which power is interrupted, but generally the contacts may open after about 1 ms. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...view of the Relays. For this reason the arrangement appears to be in reverse. Applicable model: MY Series General-purpose Relays MY Best-selling, general-purpose relays that can be s...
...tact Current The maximum contact current that can be switched. This value must not be exceeded. MY Best-selling, general-purpose relays that can be selected based on operating environment and...