| Site Search | Product Search | IA Global Search |
... microload switching. Be careful because they have different contact ratings. Contact Mechanism MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...arcing during load switching will be exceeded and the load will not be able to be disconnected. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
.... In addition, some of Relay contacts are suitable for minimum load switching and some are not. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...suppressor can be introduced as a countermeasure against discoloration caused by arc discharge. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...rry current 10 A Maximum switching voltage 250 VAC, 125 VDC Maximum switching current 10 A 10 A MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...s General-purpose Relays Bifurcated contacts: MY4Z Series, MK[]ZP Series General-purpose Relays MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...refore MY2 AC200/220V operates at 200 VAC x 80% = 160 VAC max. (when coil temperature is 23°C). MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...urs when switching a large load, and this may cause contact failure when switching a microload. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...swer Yes, the Relays may become detached if the equipments are exposed to vibration or shock. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ms such as deterioration and breakdown of the transistor caused by counter electromotive force. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
... within 20 ms. 3.Diode characteristics: Withstand inverse voltage: 1,000 V Forward current: 1 A MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...input pulse (input with inverse polarity of set input) puts the Relay into the reset condition. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...ts are suitable for operating microloads. MY4Z has a shorter electrical life. Contact Mechanism MY Best-selling, general-purpose relays that can be selected based on operating environment and...
.... FAQ02826 Related Contents Primary Contents Question Which Sockets and Hold-down Clips are for MY General-purpose Relays? Answer Refer to the following table. Connecting Sockets/Hold-down ...
...th gold-plated contacts? Answer Yes, Relays from MY4ZN-CBG General-purpose Relays, G2A, MY4Z, MY[]Q, and MY4N Series have gold-plated contacts. Even if Relays are not used and just stored, ...
...e parentheses. At 12 VDC R = 15 KΩ max. P = 450 mW min. At 24 VDC R = 30 KΩ max. P = 0.1 W min. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...10% of the coil rating. In this case, it is 121 VAC (110 VAC x 110% = 121 V). Applicable model: MY Series MY Best-selling, general-purpose relays that can be selected based on operat...
...s Primary Contents Question Do you have any Relays that can switch more than 3 A? Answer Yes, MY General-purpose Relays, LY, and MK Series. MY Best-selling, general-purpose relays ...
...t may lower the ability to dissipate heat. Use MYQ Plastic Sealed Relays or Solid-state Relays. MY Best-selling, general-purpose relays that can be selected based on operating environment and...
...-state Relays are used to operate the Relay, a reset failure may occur due to the reduced load. MY Best-selling, general-purpose relays that can be selected based on operating environment and...