| IAグローバル検索 |
.... On the model Z-15GQ8-B, the M3 hole with a depth of 10 mm is a through hole. Take precautions so that no water or screw lock agent penetrates into the hole. Panel Mount Roll...
https://www.omron-ap.com.ph/products/family/289/dimension.html
... not use both the M12 mounting screw and the mounting holes in the case at the same time. Doing so will cause stress to be applied to the Switch, possibly damaging the case or cove...
https://www.omron-ap.com.ph/products/family/291/dimension.html
...ing Bracket: Tilt the Sensor Head towards the workpiece as shown below. Adjust the installation so that the angle is 10.5° ±0.1°. * The mounting hole dimensions in parentheses (reference valu...
https://www.omron-ap.com.ph/products/family/2979/dimension.html
...92F-45 Adapter. To use the USB- Serial Conversion Cable to make the settings, do so before you mount the Temperature Controller in the panel. 4. You cannot use it tog...
https://www.omron-ap.com.ph/products/family/3101/dimension.html
...32-LD11 2M 860 360 250 110 E32-LD11R 2M 840 350 240 100 * The fiber length is 2 m on each side, so the sensing distance is given as 4,000 mm. Cylindrical Models Sensing method Size Sensing di...
https://www.omron-ap.com.ph/products/family/3103/specification.html
...D16 2M 40 to 4,200 40 to 2,100 40 to 1,350 40 to 720 *1. The fiber length is 10 m on each side, so the sensing distance is given as 20,000 mm. *2. The fiber length is 2 m on each side, ...
https://www.omron-ap.com.ph/products/family/3161/specification.html
...6 orientations. Restrictions: No restrictions Terminal connection diagram • 0V has 2 terminals, so be sure to wire both terminals. • COM (+V) has 2 terminals, so be sure to wire both...
https://www.omron-ap.com.ph/products/family/3185/specification.html
...ll dimensions. Note: With WLHAL4, WL01HAL4, WLHAL5, and WL01HAL5, the actuator's tare is large, so depending on the installation direction, they may not be properly reset. A...
https://www.omron-ap.com.ph/products/family/326/dimension.html
... characteristics Note: With WLCAL4-N, WLCAL4-LD-N and WLCAL4-LE-N the actuator's tare is large, so depending on the installation direction, they may not be properly reset. Always ins...
https://www.omron-ap.com.ph/products/family/3263/dimension.html
... SHS: Super-high-speed mode (30 μs) *2. The optical fiber is 2 m long on each side, so the sensing distance is 4,000 mm. *3. The values for the minimum sensing object are referenc...
https://www.omron-ap.com.ph/products/family/3275/lineup.html
...oller. If you reverse this order, this product will not recognize the 24V external input, so lighting greater than 7.5W will not be possible. *4. Electromagnetic environment: Industrial...
https://www.omron-ap.com.ph/products/family/3279/specification.html
...92F-45 Adapter. To use the USB- Serial Conversion Cable to make the settings, do so before you mount the Temperature Controller in the panel. 4. You cannot use this A...
https://www.omron-ap.com.ph/products/family/3288/dimension.html
...ng. If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoki...
https://www.omron-ap.com.ph/products/family/3369/specification.html
...c brake is enabled. • The dynamic brake is designed only for emergency stops. Design the system so that the Servomotor remains stopped for at least 3 minutes after applying the dynamic brake....
https://www.omron-ap.com.ph/products/family/3386/specification.html
...If the input is connected to a UPS, do not connect a UPS with a square-wave output. Doing so will cause the internal temperature of the product to increase, possibly causing smoking or ...
https://www.omron-ap.com.ph/products/family/3485/specification.html
...lue is calculated from the difference between the heights of the surface and rear surface, so there is no effect on the temperature change. ZW-S7010/S7020/S7030/S7040/SP7007/SP7010/SPR70...
https://www.omron-ap.com.ph/products/family/3500/specification.html
...before attempting a megger test (insulation resistance measurement) on a Servo Drive. Not doing so may result in the Servo Drive failure. Do not perform a dielectric strength test on the Serv...
https://www.omron-ap.com.ph/products/family/3549/specification.html
...32, 64 or 96 GB 8, 16, 32, 64 GB Memory type DDR4 (ECC is available) DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...
https://www.omron-ap.com.ph/products/family/3631/specification.html
...ion minimal 10yr) Memory Memory size *1 8, 16, 32, 64 GB Memory type DDR4 Package Memory Format SO-DIMM Serial Presence Detect (SPD) Speed grade 3200 MT/s CAS latency CL17 Trusted platform mo...
https://www.omron-ap.com.ph/products/family/3633/specification.html
...ally, turn OFF all of the pins. C SD Memory Card power supply switch Turns OFF the power supply so that you can remove the SD Memory Card. D DIN Track mounting hook These hooks are used to mo...
https://www.omron-ap.com.ph/products/family/3650/specification.html