| IAグローバル検索 |
...tal Filter This function sets the time constant applied to the first-order lag operation filter so that the noise components mixed with the measured value are eliminated. All models Measuring...
https://www.omron-ap.com/products/family/3902/specification.html
... Safety Sensors E3ZS OMRON Non-contact Safety Door Switches D40A-2, D40A Safety Output Units NX-SO Unit type Appearance Specifications Unit version Model Number of safety output points Intern...
...value (peak hold), the bottom value (bottom hold), the range of change (peak-to-peak hold), and so forth. Timer mode Allows you to delay upon changes in judgment output, or turn PASS output O...
https://www.omron-ap.com/products/family/3932/specification.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.com/products/family/3937/dimension.html
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
https://www.omron-ap.com/products/family/3938/dimension.html
...A switched and 10 A safe switched are from the same source and pass through the same 10 A fuse, so the sum of their current must be less than 10 A. Standards AMR EN IS0 12100, EN ISO 13849-1,...
https://www.omron-ap.com/products/family/3950/specification.html
...nnector. *3. However, when bending the cable to perform wiring, maintenance, and other work, do so within the temperature range of 0 to 75°C in consideration of severing of the cable. last up...
https://www.omron-ap.com/products/family/871/specification.html
...dards. How To Use It When a guard is in place, it must be designed, constructed, and maintained so that no personnel can Around, Under, Over, Through the guard. OMRON Universal Gotcha Stick m...
https://www.omron-ap.com/service-support/mseservices/gotcha-stick/
...rection. (Maintain the specified mounting space between Controllers.) • To mount the Controller so that it is waterproof, insert the waterproof packing onto the Controller. • When two or more...
...s, Ltd. --- * There is a risk of quality problems when using cables assembled by typical users, so we recommend purchasing cables with preattached connectors or having a qualified technici...
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron.co.id/products/family/1497/specification.html
...tch a standard load, it cannot be used for a load of a smaller capacity. Doing so may result in roughening of the contact surface and contact reliability may be lost. *1. The...
https://www.omron.co.id/products/family/1498/specification.html
...V E39-F1V E32-T84SV 1M (No Cutting) E32-T10V 2M (Free Cutting) E32-VF4 Note 1. Mount the Flange so that the V40 O-ring is on the atmospheric-pressure side of the vacuum chamber wall. Note 2. ...
...,000 * HS: 3,450 ST: 4,000 * SHS: 920 E32-LT11R 2M * The optical fiber is 2m long on each side, so the sensing distance is 4,000 mm. Note 1. The following mode names and response times apply ...
...2 Use these small-sized brackets when performing side mounting with standard mounting brackets, so that they do not protrude from the detection surface. 2 for an emitter, 2 for a receiver, to...
... lamp * 100 m 60 m 45 m 30 m Note: Keep the cable length within the rated length. Failure to do so is dangerous as it may prevent safety functions from operating normally. * The F39-...
https://www.omron.co.id/products/family/1581/specification.html
...termined for the current and power that can be provided to the mounted Units. Design the system so that the total current consumption for all the mounted Units does not exceed the maximum tot...
https://www.omron.co.id/products/family/1639/specification.html
...ecting Socket P3GA-11 Back Connecting Socket Note: Do not use any other types of Sockets. Doing so will adversely affect the accuracy. Applicable Thermistors Use Element Interchangeable Therm...
...Sheet). Note: Internally, inputs are processed in five ranges (refer to Table 2 on Data Sheet), so accuracy and resolution accord with these internal ranges. Example: Thermocouple: K; input r...
https://www.omron.co.id/products/family/1664/specification.html
...ed to prevent sudden process value increases due to inrush currents caused by motor startup and so on. Upper limit value: - 32,000 to 32,000 Upper limit time: 0 to 100 s Process value alarm P...
https://www.omron.co.id/products/family/1665/specification.html